<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 devices without CAAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385637#M184354</link>
    <description>&lt;P&gt;you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP&lt;/P&gt;</description>
    <pubDate>Mon, 13 Dec 2021 11:56:47 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-12-13T11:56:47Z</dc:date>
    <item>
      <title>iMX6 devices without CAAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385510#M184338</link>
      <description>&lt;P&gt;Hi, in AN12714 about Encrypted Storage using CAAM is stated: "The document applies to all i.MX SoCs having CAAM module. The feature is not available on i.MX SoCs with DCP." I searched through several product data sheets but cannot find a clear reference about "DCP" and which iMX SoCs actually do not support CAAM. Can someone help on this? Thanks, Michael&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 09:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385510#M184338</guid>
      <dc:creator>mtrx</dc:creator>
      <dc:date>2021-12-13T09:04:03Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 devices without CAAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385594#M184348</link>
      <description>&lt;P&gt;Hi, Michael&lt;/P&gt;
&lt;P&gt;I will discuss this with my other teammates which are more familiar with the 6 Series and come back with an answer ASAP.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Kind regards,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;MC&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 10:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385594#M184348</guid>
      <dc:creator>mihai_chelalau</dc:creator>
      <dc:date>2021-12-13T10:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 devices without CAAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385637#M184354</link>
      <description>&lt;P&gt;you can refer to the enclosed file, imx6ull has DCP but no CAAM which is like imx6sl, i.mx6ul doesn't support DCP&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 11:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-devices-without-CAAM/m-p/1385637#M184354</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-12-13T11:56:47Z</dc:date>
    </item>
  </channel>
</rss>