<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: I.MX8MP capture MIPI embedded data</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-capture-MIPI-embedded-data/m-p/1385187#M184310</link>
    <description>&lt;P&gt;imx8mp should have the same CSI IP as imx8mm, I checked the reference manual of imx8mm, should support 0x12 on HW, but as I known, current bsp (SW) doesn't support meta data&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 12 Dec 2021 09:14:13 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-12-12T09:14:13Z</dc:date>
    <item>
      <title>I.MX8MP capture MIPI embedded data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-capture-MIPI-embedded-data/m-p/1383845#M184171</link>
      <description>&lt;P&gt;Hi NXP Community,&lt;/P&gt;&lt;P&gt;I would like to connect a MIPI camera to a NXP I.MX8MP based board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The camera is streaming besides the actual frame data with MIPI data type 0x2A a 128 byte embedded header with 0x12 MIPI data type. It would be possible to capture the header with I.MX8MP?&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;i.MX 8M Plus Applications Processor Reference Manual, Rev. 1, 06/2021 section&amp;nbsp;13.5.6.13 0x12 data type is not in the list but I'm not sure if it is not supported or it is supported but it was not added to the list.&lt;/P&gt;&lt;P&gt;Also I would like to have, if 0x12 data type is supported, one of the ISI units configured for 0x2A DT image data on /dev/video0 capture device and second ISI channel set for 0x12 data and capture on /dev/video1&lt;/P&gt;&lt;P&gt;Do you thinnk the previous configuration is possible?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 07:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-capture-MIPI-embedded-data/m-p/1383845#M184171</guid>
      <dc:creator>btogorean</dc:creator>
      <dc:date>2021-12-09T07:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP capture MIPI embedded data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-capture-MIPI-embedded-data/m-p/1385187#M184310</link>
      <description>&lt;P&gt;imx8mp should have the same CSI IP as imx8mm, I checked the reference manual of imx8mm, should support 0x12 on HW, but as I known, current bsp (SW) doesn't support meta data&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 12 Dec 2021 09:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-capture-MIPI-embedded-data/m-p/1385187#M184310</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-12-12T09:14:13Z</dc:date>
    </item>
  </channel>
</rss>