<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx7 Sim Card Clock Speed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7-Sim-Card-Clock-Speed/m-p/1385115#M184289</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If this is still helpful for you, yes you're correct, you should modify any of the two, you may refer to the following part of the code on how it is calculated the prescaller&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc/sim/imx_sim.c?h=lf-5.10.y#n885" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc/sim/imx_sim.c?h=lf-5.10.y#n885&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;CLK_PRESCALER = (SIMn_CLK_ROOT + FCLK_FREQ - 1)/FCLK_FREQ&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Sat, 11 Dec 2021 03:16:27 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-12-11T03:16:27Z</dc:date>
    <item>
      <title>imx7 Sim Card Clock Speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-Sim-Card-Clock-Speed/m-p/1261866#M172570</link>
      <description>&lt;P&gt;I would like to know how to change the clock speed that the imx7 sim card interface generates. Currently the default clock rate is 4MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see 2 possible places where I can change that, in the device tree sim1 node or in the sim driver imx_sim.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried changing this value in the imx_sim.c file in the kernel&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define FCLK_FREQ (4000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried changing this in the device tree&lt;/P&gt;&lt;P&gt;&amp;amp;sim1 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_sim1&amp;gt;;&lt;BR /&gt;clocks = &amp;lt;&amp;amp;clks IMX7D_SIM1_ROOT_CLK&amp;gt;;&lt;BR /&gt;assigned-clock-rates = &amp;lt;240000000&amp;gt;; // this&lt;BR /&gt;pinctrl-assert-gpios = &amp;lt;&amp;amp;gpio2 4 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;port = &amp;lt;1&amp;gt;;&lt;BR /&gt;sven_high_active;&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nothing seems to have worked so far, I would like the clock rate to be 3.84MHz, any tips?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would also like to change the baud rate to the max supported by my sim card.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems I cannot put in fast uart clock rate, I know the command how to change the SIM baud rate, but for some reason the unit test mxc_simtest.c does not allow me to set di fi and the baudrate to what I want&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 09:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-Sim-Card-Clock-Speed/m-p/1261866#M172570</guid>
      <dc:creator>eoin_oconnell</dc:creator>
      <dc:date>2021-04-14T09:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx7 Sim Card Clock Speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-Sim-Card-Clock-Speed/m-p/1385115#M184289</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If this is still helpful for you, yes you're correct, you should modify any of the two, you may refer to the following part of the code on how it is calculated the prescaller&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc/sim/imx_sim.c?h=lf-5.10.y#n885" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc/sim/imx_sim.c?h=lf-5.10.y#n885&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;CLK_PRESCALER = (SIMn_CLK_ROOT + FCLK_FREQ - 1)/FCLK_FREQ&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 11 Dec 2021 03:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-Sim-Card-Clock-Speed/m-p/1385115#M184289</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-12-11T03:16:27Z</dc:date>
    </item>
  </channel>
</rss>