<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8 shared (USB) peripherals between cores</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-shared-USB-peripherals-between-cores/m-p/1385058#M184280</link>
    <description>&lt;P&gt;I have a suspicion the answer may be no "no", but is there any possible way to share a single USB host peripheral between the two i.MX8 cores (A53 and M7)?&amp;nbsp; Ideally, the A53 talking to a USB camera and the M7 communicating via VCP, over a single USB cable.&amp;nbsp; The A53 will be running Linux or Android - which I suspect is what may preclude this... I'm thinking any attempt to put something else in control of the USB host (with a mutex or such) will probably break the V4L2 connection...?&lt;/P&gt;&lt;P&gt;More generally, can less-sophisticated peripherals (such as GPIO, I2C, UART, etc) be shared (with mutex perhaps) between both cores?&lt;/P&gt;</description>
    <pubDate>Fri, 10 Dec 2021 21:03:12 GMT</pubDate>
    <dc:creator>Earthshine</dc:creator>
    <dc:date>2021-12-10T21:03:12Z</dc:date>
    <item>
      <title>i.MX8 shared (USB) peripherals between cores</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-shared-USB-peripherals-between-cores/m-p/1385058#M184280</link>
      <description>&lt;P&gt;I have a suspicion the answer may be no "no", but is there any possible way to share a single USB host peripheral between the two i.MX8 cores (A53 and M7)?&amp;nbsp; Ideally, the A53 talking to a USB camera and the M7 communicating via VCP, over a single USB cable.&amp;nbsp; The A53 will be running Linux or Android - which I suspect is what may preclude this... I'm thinking any attempt to put something else in control of the USB host (with a mutex or such) will probably break the V4L2 connection...?&lt;/P&gt;&lt;P&gt;More generally, can less-sophisticated peripherals (such as GPIO, I2C, UART, etc) be shared (with mutex perhaps) between both cores?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 21:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-shared-USB-peripherals-between-cores/m-p/1385058#M184280</guid>
      <dc:creator>Earthshine</dc:creator>
      <dc:date>2021-12-10T21:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 shared (USB) peripherals between cores</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-shared-USB-peripherals-between-cores/m-p/1385087#M184283</link>
      <description>&lt;P&gt;Hi Brian&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;unfortunately answer is no. The only solution to share some module between M4/7 and A53&lt;/P&gt;
&lt;P&gt;is to implement a client-server approach using RPMSG and only one core to program module.&lt;/P&gt;
&lt;P&gt;i.MX7ULP MCUXpresso SDK includes some examples of access service via RPMSG on the M4 side .&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/i2c/busses/i2c-rpmsg-imx.c?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/i2c/busses/i2c-rpmsg-imx.c?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 23:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-shared-USB-peripherals-between-cores/m-p/1385087#M184283</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-12-10T23:56:39Z</dc:date>
    </item>
  </channel>
</rss>