<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Serial communication using one wire mode (half duplex)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Serial-communication-using-one-wire-mode-half-duplex/m-p/1383729#M184161</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194474"&gt;@Hellspread41&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You can check the RT1062 LPSPI module, half-duplex function,.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You also can check the LPUART, chapter 49.3.6.4 Single-wire operation&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;49.3.6.4 Single-wire operation&lt;BR /&gt;When CTRL[LOOPS] is set, the CTRL[RSRC] bit chooses between loop mode&lt;BR /&gt;(CTRL[RSRC] = 0) or single-wire mode (CTRL[RSRC] = 1). Single-wire mode&lt;BR /&gt;implements a half-duplex serial connection. The receiver is internally connected to the&lt;BR /&gt;transmitter output and to the TXD pin (the RXD pin is not used).&lt;BR /&gt;In single-wire mode, the CTRL[TXDIR] bit controls the direction of serial data on the&lt;BR /&gt;TXD pin. When CTRL[TXDIR] is cleared, the TXD pin is an input to the receiver and&lt;BR /&gt;the transmitter is temporarily disconnected from the TXD pin so an external device can&lt;BR /&gt;send serial data to the receiver. When CTRL[TXDIR] is set, the TXD pin is an output&lt;BR /&gt;driven by the transmitter, the internal loop back connection is disabled, and as a result the&lt;BR /&gt;receiver cannot receive characters that are sent out by the transmitter.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;If you still have questions about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
    <pubDate>Thu, 09 Dec 2021 03:25:13 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2021-12-09T03:25:13Z</dc:date>
    <item>
      <title>Serial communication using one wire mode (half duplex)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-communication-using-one-wire-mode-half-duplex/m-p/1382858#M184091</link>
      <description>&lt;P&gt;Hello all, just wondering if someone has an exemple on how to setup a serial com in half duplex mode. according the datasheet of imxrt 1062 it is possible to do it but don't really know how to make it work ? thx&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 20:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-communication-using-one-wire-mode-half-duplex/m-p/1382858#M184091</guid>
      <dc:creator>Hellspread41</dc:creator>
      <dc:date>2021-12-07T20:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: Serial communication using one wire mode (half duplex)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-communication-using-one-wire-mode-half-duplex/m-p/1383729#M184161</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194474"&gt;@Hellspread41&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You can check the RT1062 LPSPI module, half-duplex function,.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You also can check the LPUART, chapter 49.3.6.4 Single-wire operation&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;49.3.6.4 Single-wire operation&lt;BR /&gt;When CTRL[LOOPS] is set, the CTRL[RSRC] bit chooses between loop mode&lt;BR /&gt;(CTRL[RSRC] = 0) or single-wire mode (CTRL[RSRC] = 1). Single-wire mode&lt;BR /&gt;implements a half-duplex serial connection. The receiver is internally connected to the&lt;BR /&gt;transmitter output and to the TXD pin (the RXD pin is not used).&lt;BR /&gt;In single-wire mode, the CTRL[TXDIR] bit controls the direction of serial data on the&lt;BR /&gt;TXD pin. When CTRL[TXDIR] is cleared, the TXD pin is an input to the receiver and&lt;BR /&gt;the transmitter is temporarily disconnected from the TXD pin so an external device can&lt;BR /&gt;send serial data to the receiver. When CTRL[TXDIR] is set, the TXD pin is an output&lt;BR /&gt;driven by the transmitter, the internal loop back connection is disabled, and as a result the&lt;BR /&gt;receiver cannot receive characters that are sent out by the transmitter.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;If you still have questions about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 03:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-communication-using-one-wire-mode-half-duplex/m-p/1383729#M184161</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-12-09T03:25:13Z</dc:date>
    </item>
  </channel>
</rss>