<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HAB authenticate image callback usage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1382733#M184077</link>
    <description>&lt;P&gt;Hello, thanks for the answer.&lt;/P&gt;&lt;P&gt;I took care of the warnings you posted and tried to find the answer to my question in the HAB4_API.pdf. In the document it is stated that the callback function is called between the dcd and the csf. As far as I understood, that means that the callback function is called before authentication happens. Is that right?&lt;/P&gt;</description>
    <pubDate>Tue, 07 Dec 2021 14:25:16 GMT</pubDate>
    <dc:creator>DanielD</dc:creator>
    <dc:date>2021-12-07T14:25:16Z</dc:date>
    <item>
      <title>HAB authenticate image callback usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1381232#M183937</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working on implementing Secure Boot on a Board based on the i.MX8M Mini. I tried to use the hab_rvt_authenticate_image() function which worked. Now I wanted to implement a callback function. The problem is that I don't understand when exactly the callback function is called. No matter if I write it as if it is called before or after authetication, I get an Invalid IVT Event, which isn't happening if I don't use the callback and copy manually.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With that said, my questions are:&lt;/P&gt;&lt;P&gt;1) When is the callback called, befor or after authentication?&lt;/P&gt;&lt;P&gt;2) Do I miss something about the intended usage?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 11:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1381232#M183937</guid>
      <dc:creator>DanielD</dc:creator>
      <dc:date>2021-12-03T11:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: HAB authenticate image callback usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1382260#M184043</link>
      <description>&lt;P&gt;Please see&amp;nbsp;HAB4_API.pdf&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Warnings:
• The loader callback function should lie within existing authenticated areas.
• It is the responsibility of the caller to check the initial image load addresses using hab_rvt.check_target() prior to loading the initial image and calling this function.
• After completion of hab_rvt.authenticate_image(), the caller should test using hab_rvt.assert() that the Boot Data was authenticated.
• After completion of hab_rvt.authenticate_image(), the caller should test using hab_rvt.assert() that the Boot Data was authenticated&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 02:12:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1382260#M184043</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-12-07T02:12:10Z</dc:date>
    </item>
    <item>
      <title>Re: HAB authenticate image callback usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1382733#M184077</link>
      <description>&lt;P&gt;Hello, thanks for the answer.&lt;/P&gt;&lt;P&gt;I took care of the warnings you posted and tried to find the answer to my question in the HAB4_API.pdf. In the document it is stated that the callback function is called between the dcd and the csf. As far as I understood, that means that the callback function is called before authentication happens. Is that right?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 14:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-authenticate-image-callback-usage/m-p/1382733#M184077</guid>
      <dc:creator>DanielD</dc:creator>
      <dc:date>2021-12-07T14:25:16Z</dc:date>
    </item>
  </channel>
</rss>