<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bare metal applications on the Cortex-A7 core of the MCIMX7ULP-EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379027#M183755</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently developing bare metal applications on the Cortex-A7 core of the&amp;nbsp;MCIMX7ULP-EVK and have been having some issues with initial debugging via JTAG/SWD.&lt;/P&gt;&lt;P&gt;I have to stop at the uboot prompt to be able to download/debug my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an available configuration of the boot options of the&amp;nbsp;MCIMX7ULP-EVK that will allow me to download/debug an application via JTAG/SWD?&lt;/P&gt;&lt;P&gt;What is the most convenient way to download/debug code via JTAG/SWD?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Obi&lt;/P&gt;</description>
    <pubDate>Tue, 30 Nov 2021 14:09:18 GMT</pubDate>
    <dc:creator>aghogho_obi</dc:creator>
    <dc:date>2021-11-30T14:09:18Z</dc:date>
    <item>
      <title>Bare metal applications on the Cortex-A7 core of the MCIMX7ULP-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379027#M183755</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently developing bare metal applications on the Cortex-A7 core of the&amp;nbsp;MCIMX7ULP-EVK and have been having some issues with initial debugging via JTAG/SWD.&lt;/P&gt;&lt;P&gt;I have to stop at the uboot prompt to be able to download/debug my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an available configuration of the boot options of the&amp;nbsp;MCIMX7ULP-EVK that will allow me to download/debug an application via JTAG/SWD?&lt;/P&gt;&lt;P&gt;What is the most convenient way to download/debug code via JTAG/SWD?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Obi&lt;/P&gt;</description>
      <pubDate>Tue, 30 Nov 2021 14:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379027#M183755</guid>
      <dc:creator>aghogho_obi</dc:creator>
      <dc:date>2021-11-30T14:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Bare metal applications on the Cortex-A7 core of the MCIMX7ULP-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379713#M183828</link>
      <description>&lt;P&gt;Hello aghogho_obi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We using the Realview ICE for debugging in bare metal and JTAG.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 01 Dec 2021 13:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379713#M183828</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-12-01T13:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Bare metal applications on the Cortex-A7 core of the MCIMX7ULP-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379735#M183829</link>
      <description>&lt;P&gt;Thank you, one question though:&lt;/P&gt;&lt;P&gt;What boot switch configuration or any other configuration of the MCIMX7ULP-EVK do you recommend for baremetal development on the Cortex-A7?&lt;/P&gt;&lt;P&gt;So far, JTAG/SWD is only accessible when I stop at uboot. When the&amp;nbsp;MCIMX7ULP-EVK is in the USB Downloader mode, I cannot access the Cortex-A7 from JTAG/SWD. For other iMX boards, I can access JTAG/SWD in this mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Dec 2021 13:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1379735#M183829</guid>
      <dc:creator>aghogho_obi</dc:creator>
      <dc:date>2021-12-01T13:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: Bare metal applications on the Cortex-A7 core of the MCIMX7ULP-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1389088#M184689</link>
      <description>&lt;P&gt;Do I have to stop the boot process during uboot to be able to debug/program the cortex-A7? Is there another way to do this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Still waiting for a response on this....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 19 Dec 2021 12:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bare-metal-applications-on-the-Cortex-A7-core-of-the-MCIMX7ULP/m-p/1389088#M184689</guid>
      <dc:creator>aghogho_obi</dc:creator>
      <dc:date>2021-12-19T12:40:27Z</dc:date>
    </item>
  </channel>
</rss>