<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 88W8887 WIFI Not able to start AP/STA mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/88W8887-WIFI-Not-able-to-start-AP-STA-mode/m-p/1377433#M183571</link>
    <description>&lt;P&gt;Dear sir/mam,&lt;/P&gt;&lt;P&gt;We are trying to do integration of Vendor HAL and drivers of WLAN and BT on Android Q platform with attached text file below named as wifi_readme.&lt;/P&gt;&lt;P&gt;1) Once the module got loaded using the following command&lt;BR /&gt;insmod vendor/lib/modules/mlan.ko&lt;BR /&gt;insmod vendor/lib/modules/sd8xxx.ko fw_name=nxp/sd8887_wlan_a2.bin cal_data_cfg=none cfg80211_wext=0xf sta_name=wlan wfd_name=p2p drv_mode=0x5 in early_init.cfg while booting.&lt;/P&gt;&lt;P&gt;2) Firmware also got download successfully with below prints&lt;BR /&gt;[ 9.088675] Wlan: FW download over, firmwarelen=399832 downloaded 399832&lt;BR /&gt;[ 9.544094] WLAN FW is active&lt;BR /&gt;[ 9.547082] on_time is 9407047750&lt;/P&gt;&lt;P&gt;3) While setting cfg80211_wext=0xf, we are getting kernel crash related to CFG80211 module.&lt;BR /&gt;&lt;BR /&gt;4) If the cfg80211_wext is not passed while inserting the module using the command:&lt;BR /&gt;insmod vendor/lib/modules/sd8xxx.ko fw_name=nxp/sd8887_wlan_a2.bin cal_data_cfg=none sta_name=wlan wfd_name=p2p drv_mode=0x5. Then the interface for both station and ap mode is up and crash is not happening. But, wifi scan is not happening ie both ap and STA mode is not working while testing with android UI.&lt;/P&gt;&lt;P&gt;Interface prints:&lt;BR /&gt;uap0 Link encap:Ethernet HWaddr 48:a4:93:49:13:3c Driver wlan_sdio&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;wlan0 Link encap:Ethernet HWaddr 48:a4:93:49:12:3c Driver wlan_sdio&lt;BR /&gt;BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;5) The platform and Wireless chipset mentioned below are used.&lt;/P&gt;&lt;P&gt;NXP Board : i.MX8QXP&lt;BR /&gt;Android Q10.0.0_2.6.0 (Linux 5.4.70 kernel)&lt;BR /&gt;Wireless Chipset : 88W8887&lt;BR /&gt;Package_verison:SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p32-15.100.19.p32-C4X15647_A2-GPL&lt;BR /&gt;Vendor HAL : V007 Version&lt;/P&gt;&lt;P&gt;6) Attached the error_log below, named as wifi_crash_log for reference.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Kindly help on this issue. Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Afridi,&lt;BR /&gt;Zumi solutions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Nov 2021 06:57:19 GMT</pubDate>
    <dc:creator>afridi20</dc:creator>
    <dc:date>2021-11-26T06:57:19Z</dc:date>
    <item>
      <title>88W8887 WIFI Not able to start AP/STA mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/88W8887-WIFI-Not-able-to-start-AP-STA-mode/m-p/1377433#M183571</link>
      <description>&lt;P&gt;Dear sir/mam,&lt;/P&gt;&lt;P&gt;We are trying to do integration of Vendor HAL and drivers of WLAN and BT on Android Q platform with attached text file below named as wifi_readme.&lt;/P&gt;&lt;P&gt;1) Once the module got loaded using the following command&lt;BR /&gt;insmod vendor/lib/modules/mlan.ko&lt;BR /&gt;insmod vendor/lib/modules/sd8xxx.ko fw_name=nxp/sd8887_wlan_a2.bin cal_data_cfg=none cfg80211_wext=0xf sta_name=wlan wfd_name=p2p drv_mode=0x5 in early_init.cfg while booting.&lt;/P&gt;&lt;P&gt;2) Firmware also got download successfully with below prints&lt;BR /&gt;[ 9.088675] Wlan: FW download over, firmwarelen=399832 downloaded 399832&lt;BR /&gt;[ 9.544094] WLAN FW is active&lt;BR /&gt;[ 9.547082] on_time is 9407047750&lt;/P&gt;&lt;P&gt;3) While setting cfg80211_wext=0xf, we are getting kernel crash related to CFG80211 module.&lt;BR /&gt;&lt;BR /&gt;4) If the cfg80211_wext is not passed while inserting the module using the command:&lt;BR /&gt;insmod vendor/lib/modules/sd8xxx.ko fw_name=nxp/sd8887_wlan_a2.bin cal_data_cfg=none sta_name=wlan wfd_name=p2p drv_mode=0x5. Then the interface for both station and ap mode is up and crash is not happening. But, wifi scan is not happening ie both ap and STA mode is not working while testing with android UI.&lt;/P&gt;&lt;P&gt;Interface prints:&lt;BR /&gt;uap0 Link encap:Ethernet HWaddr 48:a4:93:49:13:3c Driver wlan_sdio&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;wlan0 Link encap:Ethernet HWaddr 48:a4:93:49:12:3c Driver wlan_sdio&lt;BR /&gt;BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 TX bytes:0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;5) The platform and Wireless chipset mentioned below are used.&lt;/P&gt;&lt;P&gt;NXP Board : i.MX8QXP&lt;BR /&gt;Android Q10.0.0_2.6.0 (Linux 5.4.70 kernel)&lt;BR /&gt;Wireless Chipset : 88W8887&lt;BR /&gt;Package_verison:SD-WLAN-UART-BT-8887-U16-MMC-W15.87.19.p32-15.100.19.p32-C4X15647_A2-GPL&lt;BR /&gt;Vendor HAL : V007 Version&lt;/P&gt;&lt;P&gt;6) Attached the error_log below, named as wifi_crash_log for reference.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Kindly help on this issue. Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Afridi,&lt;BR /&gt;Zumi solutions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 06:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/88W8887-WIFI-Not-able-to-start-AP-STA-mode/m-p/1377433#M183571</guid>
      <dc:creator>afridi20</dc:creator>
      <dc:date>2021-11-26T06:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8887 WIFI Not able to start AP/STA mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/88W8887-WIFI-Not-able-to-start-AP-STA-mode/m-p/1377566#M183588</link>
      <description>&lt;P&gt;Hi Afridi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;only 88W8997 is oficially supported in Android Q10.0.0_2.6.0 for i.MX8QXP&lt;/P&gt;
&lt;P&gt;as described in Release Notes included in &lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/webapp/Download?colCode=Q10.0.0_2.6.0_DOCS" data-dtmsubaction="Documentation​ link" target="_blank"&gt;Documentation​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In general one can try steps provided in sect.2.2 Configure and start the Access Point UM11490&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_3" href="https://www.nxp.com/webapp/Download?colCode=UM11490" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK - User manual (public)&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 10:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/88W8887-WIFI-Not-able-to-start-AP-STA-mode/m-p/1377566#M183588</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-26T10:04:47Z</dc:date>
    </item>
  </channel>
</rss>