<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1377089#M183543</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks a lot for the provided links&lt;/P&gt;&lt;P&gt;We are actually looking for the revision comparison document between silicon v1.3 and v1.4&lt;/P&gt;&lt;P&gt;This is needed to fix the secured u-boot lockup that we are facing now.&lt;/P&gt;&lt;P&gt;We currently using u-boot and SPL from&amp;nbsp;2016.09 and after soldering new processor v1.4 (HAB v4.2) the SPL refuses to boot.&lt;/P&gt;&lt;P&gt;We see this messages:&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xcc, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x2c 0x42 0x33 0x30 0xe1 0x1e&lt;BR /&gt;0x00 0x00 0x00 0x00 0x80 0x00 0x0b 0x00&lt;BR /&gt;0x00 0x00 0x00 0x02 0x00 0x00 0x00 0x20&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x08 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_SNVS (0x1E)&lt;/P&gt;&lt;P&gt;We are on the way to update the u-boot to version&amp;nbsp;2020.01-rc1 and I hope it will just start working, but I would like to know the revision change details.&lt;/P&gt;&lt;P&gt;Thanks is advance,&lt;/P&gt;</description>
    <pubDate>Thu, 25 Nov 2021 13:14:04 GMT</pubDate>
    <dc:creator>Virviglaz</dc:creator>
    <dc:date>2021-11-25T13:14:04Z</dc:date>
    <item>
      <title>Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1376309#M183492</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Looking for a document&lt;/P&gt;&lt;P&gt;i.MX 6Solo/6DualLite Application Processor&amp;nbsp;Silicon Revision 1.3 to 1.4 Comparison&lt;/P&gt;&lt;P&gt;Thanks is advance,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 11:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1376309#M183492</guid>
      <dc:creator>Virviglaz</dc:creator>
      <dc:date>2021-11-24T11:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1376377#M183501</link>
      <description>&lt;P&gt;Hello Virviglaz,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no EB804, but you can fin the errata on this document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-Vybrid-Security-Vulnerability-Errata-ERR010872-ERR010873/ta-p/1120527" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-Vybrid-Security-Vulnerability-Errata-ERR010872-ERR010873/ta-p/1120527&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/errata/IMX6SXCE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/errata/IMX6SXCE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 14:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1376377#M183501</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-11-24T14:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1377089#M183543</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks a lot for the provided links&lt;/P&gt;&lt;P&gt;We are actually looking for the revision comparison document between silicon v1.3 and v1.4&lt;/P&gt;&lt;P&gt;This is needed to fix the secured u-boot lockup that we are facing now.&lt;/P&gt;&lt;P&gt;We currently using u-boot and SPL from&amp;nbsp;2016.09 and after soldering new processor v1.4 (HAB v4.2) the SPL refuses to boot.&lt;/P&gt;&lt;P&gt;We see this messages:&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xcc, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x2c 0x42 0x33 0x30 0xe1 0x1e&lt;BR /&gt;0x00 0x00 0x00 0x00 0x80 0x00 0x0b 0x00&lt;BR /&gt;0x00 0x00 0x00 0x02 0x00 0x00 0x00 0x20&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x08 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00&lt;/P&gt;&lt;P&gt;STS = HAB_FAILURE (0x33)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_SNVS (0x1E)&lt;/P&gt;&lt;P&gt;We are on the way to update the u-boot to version&amp;nbsp;2020.01-rc1 and I hope it will just start working, but I would like to know the revision change details.&lt;/P&gt;&lt;P&gt;Thanks is advance,&lt;/P&gt;</description>
      <pubDate>Thu, 25 Nov 2021 13:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-EB804-Application-Processor-Silicon-Revision-from-1/m-p/1377089#M183543</guid>
      <dc:creator>Virviglaz</dc:creator>
      <dc:date>2021-11-25T13:14:04Z</dc:date>
    </item>
  </channel>
</rss>