<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MP NAND SECURE BOOT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376265#M183484</link>
    <description>&lt;P&gt;Okay, thank you Igor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have achieved NAND secure boot indeed, BUT without the uboot commands available to manage the HAB, this is, disabling the CONFIG_IMX_HAB. Is there any path that let me use the CONFIG_IMX_HAB define while implementing the secure boot from a NAND.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Wed, 24 Nov 2021 10:32:15 GMT</pubDate>
    <dc:creator>AlfTeleco</dc:creator>
    <dc:date>2021-11-24T10:32:15Z</dc:date>
    <item>
      <title>IMX8MP NAND SECURE BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1375483#M183422</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to achieve secure boot, booting from a NAND memory. I'd been able to do it from an SD, so usual steps as signing, creating the PKI and CSF files are well formed and are familiar to me.&amp;nbsp;&lt;/P&gt;&lt;P&gt;As far as I could see, there is a problem conforming the final binary with the addresses according to this thread:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://lists.denx.de/pipermail/u-boot/2019-December/394629.html" target="_blank"&gt;https://lists.denx.de/pipermail/u-boot/2019-December/394629.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The only existing solution to finally perform a secure boot from NAND is to disable CONFIG_IMX_HAB, and by doing so we loose the ability to check HAB events and the power of the HAB commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any news in this topic? Any uboot patch that I have not been able to find?&lt;/P&gt;&lt;P&gt;Thank in advance&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 08:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1375483#M183422</guid>
      <dc:creator>AlfTeleco</dc:creator>
      <dc:date>2021-11-23T08:44:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP NAND SECURE BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376197#M183478</link>
      <description>&lt;P&gt;Hi Alvaro&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;nand secure boot is supported, there are no additional patches for that.&lt;/P&gt;
&lt;P&gt;However there is below implication for latest kernels&lt;/P&gt;
&lt;P&gt;&lt;A href="https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/commit/?id=b5094b7f135be" target="_blank"&gt;https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/commit/?id=b5094b7f135be&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 09:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376197#M183478</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-24T09:45:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP NAND SECURE BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376265#M183484</link>
      <description>&lt;P&gt;Okay, thank you Igor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have achieved NAND secure boot indeed, BUT without the uboot commands available to manage the HAB, this is, disabling the CONFIG_IMX_HAB. Is there any path that let me use the CONFIG_IMX_HAB define while implementing the secure boot from a NAND.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 10:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376265#M183484</guid>
      <dc:creator>AlfTeleco</dc:creator>
      <dc:date>2021-11-24T10:32:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP NAND SECURE BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376322#M183495</link>
      <description>&lt;P&gt;what uboot used in the case, one can try nxp from &lt;A href="https://source.codeaurora.org/external/imx/uboot-imx" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx&lt;/A&gt;&amp;nbsp; repository&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=lf_v2021.04" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=lf_v2021.04&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;follow documentation :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_secure_boot.txt?h=lf_v2021.04" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_secure_boot.txt?h=lf_v2021.04&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 12:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-NAND-SECURE-BOOT/m-p/1376322#M183495</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-24T12:24:59Z</dc:date>
    </item>
  </channel>
</rss>