<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSD card detection with multiplexed CD/DAT3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-detection-with-multiplexed-CD-DAT3/m-p/234466#M18347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to detect an SD card insertion / removal with a micro-SD socket with multiplexed CD / DAT3 line, in Linux on i.MX6 ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Sep 2013 13:48:17 GMT</pubDate>
    <dc:creator>andreygelman</dc:creator>
    <dc:date>2013-09-16T13:48:17Z</dc:date>
    <item>
      <title>SD card detection with multiplexed CD/DAT3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-detection-with-multiplexed-CD-DAT3/m-p/234466#M18347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to detect an SD card insertion / removal with a micro-SD socket with multiplexed CD / DAT3 line, in Linux on i.MX6 ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2013 13:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-card-detection-with-multiplexed-CD-DAT3/m-p/234466#M18347</guid>
      <dc:creator>andreygelman</dc:creator>
      <dc:date>2013-09-16T13:48:17Z</dc:date>
    </item>
    <item>
      <title>Re: SD card detection with multiplexed CD/DAT3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-detection-with-multiplexed-CD-DAT3/m-p/234467#M18348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CD/DAT3 card detection mechanism is workable on i.MX6, but there is no well-implementation of SDHC bus driver.&lt;/P&gt;&lt;P&gt;You can set uSDHCx_INT_STATUS_EN:CINSSEN, uSDHCx_INT_SIGNAL_EN:CINSIEN, and uSDHCx_PROT_CTRL:D3CD to enable CD/DAT3 card detection mechanism. Before that, you need to configure SD_DAT3 pad with pull-down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it's preferred to use mechanism switch(GPIO) for card detection, DAT3 is CS pin for SPI mode. A pull-down on this pin and CMD0 may set this card into the SPI mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2013 03:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-card-detection-with-multiplexed-CD-DAT3/m-p/234467#M18348</guid>
      <dc:creator>max_tsai</dc:creator>
      <dc:date>2013-09-25T03:14:18Z</dc:date>
    </item>
  </channel>
</rss>