<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: System halt during DDR calibration. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/System-halt-during-DDR-calibration/m-p/234457#M18338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure your code is really in IRAM? Do you have your own setup code with DCD headers or did you modify u-boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe u-boot will enable MMU unit very early so you need to keep that in mind when accessing memory regions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2013 08:44:49 GMT</pubDate>
    <dc:creator>VladanJovanovic</dc:creator>
    <dc:date>2013-01-24T08:44:49Z</dc:date>
    <item>
      <title>System halt during DDR calibration.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-halt-during-DDR-calibration/m-p/234456#M18337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm wondering how to properly calibrate the DDR via MMDC once the system is up and running (i.e. after exiting DCD and starting the application).&lt;/P&gt;&lt;P&gt;Directly after my boot ROM copied and started the application code, I initialize my console to see what's up, copy the calibration code to IRAM and start execution of the calibration code.&lt;/P&gt;&lt;P&gt;As soon as I set the MMDC MDSCR register bit CON_REQ to 0x1 (config request) and CMD to 0x2 (auto-refresh) (0x8020), the system seems to halt, I can't even poll the CON_ACK bit.&lt;/P&gt;&lt;P&gt;Any ideas what's going on?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2013 11:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-halt-during-DDR-calibration/m-p/234456#M18337</guid>
      <dc:creator>danielmi</dc:creator>
      <dc:date>2013-01-23T11:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: System halt during DDR calibration.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-halt-during-DDR-calibration/m-p/234457#M18338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure your code is really in IRAM? Do you have your own setup code with DCD headers or did you modify u-boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe u-boot will enable MMU unit very early so you need to keep that in mind when accessing memory regions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 08:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-halt-during-DDR-calibration/m-p/234457#M18338</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-01-24T08:44:49Z</dc:date>
    </item>
  </channel>
</rss>