<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mn uuu Waiting for /dev/utp to appear in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1374615#M183327</link>
    <description>&lt;P&gt;Hi Andy&lt;/P&gt;&lt;P&gt;Have you fixed this issue?&lt;/P&gt;&lt;P&gt;I have the same problem with uuu to download to my imx8mm EVK?&lt;/P&gt;&lt;P&gt;I also use the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;linux5.4 kernel , can't find&amp;nbsp;CONFIG_FSL_UTP either.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It can't enter into FBK mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 20 Nov 2021 15:34:26 GMT</pubDate>
    <dc:creator>imx8-mdt</dc:creator>
    <dc:date>2021-11-20T15:34:26Z</dc:date>
    <item>
      <title>imx8mn uuu Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1289781#M175258</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My CPU is IMX8MN, and the linux kernel version is linux-5.4.70. Use the kernel I compiled for uuu programming. The crotex-A serial port print information is as follows:&lt;/P&gt;&lt;P&gt;Run /linuxrc as init process&lt;BR /&gt;Found New UDC: ci_hdrc.0&lt;BR /&gt;ci_hdrc.0 0&lt;BR /&gt;ffs.utp0&lt;BR /&gt;file system registered&lt;BR /&gt;Mass Storage Function, version: 2009/09/11&lt;BR /&gt;LUN: removable file: (no medium)&lt;BR /&gt;run utp at /dev/usb-utp0/ep0[ 3.595243] read descriptors&lt;/P&gt;&lt;P&gt;.&lt;BR /&gt;uuu fastboot client 1.0.0 [b[ 3.598887] read strings&lt;BR /&gt;uilt Dec 16 2020 14:04:17]&lt;BR /&gt;Start init usb&lt;BR /&gt;write string&lt;BR /&gt;Start handle command&lt;BR /&gt;uuc /dev/utp&lt;BR /&gt;uuc 0.6 [built Dec 16 2020 14:04:17]&lt;BR /&gt;UTP: Waiting for /dev/utp to appear&lt;/P&gt;&lt;P&gt;Then it crashed。&lt;/P&gt;&lt;P&gt;CMD window information is as follows:&lt;/P&gt;&lt;P&gt;E:\ubuntu-ssh\imx8mn\linux5.4.70&amp;gt;uuu -v uuu.auto&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDPS: boot -f flash.bin&lt;BR /&gt;100%2:2&amp;gt;Okay (3.087s)&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;2:2&amp;gt;Okay (0.016s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;2:2&amp;gt;Okay (0.197s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: flash bootloader flash.bin&lt;BR /&gt;0x400000002:2&amp;gt;Okay (0.226s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;2:2&amp;gt;Okay (0.019s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;2:2&amp;gt;Okay (0.006s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi&lt;BR /&gt;2:2&amp;gt;Okay (0.007s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv emmc_cmd mmc bootbus ${emmc_dev} 2 2 1;&lt;BR /&gt;2:2&amp;gt;Okay (0.005s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi&lt;BR /&gt;2:2&amp;gt;Okay (0.01s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}&lt;BR /&gt;2:2&amp;gt;Okay (0.008s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: download -f Image&lt;BR /&gt;2:2&amp;gt;Okay (0.748s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr}&lt;BR /&gt;2:2&amp;gt;Okay (0.008s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: download -f imx8mn-ddr4-evk.dtb&lt;BR /&gt;2:2&amp;gt;Okay (0.013s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr}&lt;BR /&gt;2:2&amp;gt;Okay (0.007s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: download -f fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot&lt;BR /&gt;2:2&amp;gt;Okay (0.377s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}&lt;BR /&gt;2:2&amp;gt;Okay (0.003s)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to solve this problem？&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 08:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1289781#M175258</guid>
      <dc:creator>andy9</dc:creator>
      <dc:date>2021-06-09T08:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mn uuu Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1289852#M175270</link>
      <description>&lt;P&gt;Hi yongqiang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;had board passed ddr test, if not first recommended to run ddr test (also use RPA tool) and rebuild image&lt;/P&gt;
&lt;P&gt;as described in ddr test documentation&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 10:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1289852#M175270</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-09T10:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mn uuu Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1291032#M175374</link>
      <description>&lt;P&gt;I have tested it, Calibration is successful, and the "ddr4_timing.c" file is also replaced. It's still stuck there now.&lt;/P&gt;&lt;P&gt;①、When I use the "uuu -lsusb" command, I found that imx8mn has been in the FB state and did not enter the FBK mode.&lt;/P&gt;&lt;P&gt;②、In the linux5.4 kernel, neither the CONFIG_FSL_UTP configuration item nor the "kernel/drivers/usb/gadget/function/fsl_updater.c" file was found. This is used to upgrade in imx7d-linux4.1.15. Does imx8mn-linux5.4 need this file? Provide a patch if need,Please.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 02:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1291032#M175374</guid>
      <dc:creator>andy9</dc:creator>
      <dc:date>2021-06-11T02:54:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mn uuu Waiting for /dev/utp to appear</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1374615#M183327</link>
      <description>&lt;P&gt;Hi Andy&lt;/P&gt;&lt;P&gt;Have you fixed this issue?&lt;/P&gt;&lt;P&gt;I have the same problem with uuu to download to my imx8mm EVK?&lt;/P&gt;&lt;P&gt;I also use the&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;linux5.4 kernel , can't find&amp;nbsp;CONFIG_FSL_UTP either.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It can't enter into FBK mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 20 Nov 2021 15:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mn-uuu-Waiting-for-dev-utp-to-appear/m-p/1374615#M183327</guid>
      <dc:creator>imx8-mdt</dc:creator>
      <dc:date>2021-11-20T15:34:26Z</dc:date>
    </item>
  </channel>
</rss>