<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 I2C demo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2C-demo/m-p/1374503#M183309</link>
    <description>&lt;P&gt;Hello! I'm trying to learn more about i2c and have imported an SDK example to assisting in the learning process. Although I've run into some issues debugging/running the demo. The debug console will display some of what the demo is suppose to print on the Serial COM terminal I have opened but then it hangs and never makes it to the rest of the demo. I stepped through the demo and it is stuck on a while loop that is waiting for the slave to finish receiving (while(g_SlaveRxIndex &amp;lt; LPI2C_DATA_LENGTH)). It was the lpi2c interrupt demo, which didn't come with separate master/slave code so I assumed the demo would run on my board without any additional peripherals.&lt;/P&gt;&lt;P&gt;I'm new to embedded systems coding, any insight would be helpful.&lt;/P&gt;&lt;P&gt;Board is: MIMXRT1170-EVK&lt;/P&gt;&lt;P&gt;SDK is: SDK_2.x_MIMXRT1170-EVK (SDK Version 2.10.1)&lt;/P&gt;&lt;P&gt;Demo is: evkmimxrt1170_lpi2c_interrupt_cm7&lt;/P&gt;</description>
    <pubDate>Fri, 19 Nov 2021 17:30:03 GMT</pubDate>
    <dc:creator>CMoran</dc:creator>
    <dc:date>2021-11-19T17:30:03Z</dc:date>
    <item>
      <title>I2C demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-demo/m-p/1374503#M183309</link>
      <description>&lt;P&gt;Hello! I'm trying to learn more about i2c and have imported an SDK example to assisting in the learning process. Although I've run into some issues debugging/running the demo. The debug console will display some of what the demo is suppose to print on the Serial COM terminal I have opened but then it hangs and never makes it to the rest of the demo. I stepped through the demo and it is stuck on a while loop that is waiting for the slave to finish receiving (while(g_SlaveRxIndex &amp;lt; LPI2C_DATA_LENGTH)). It was the lpi2c interrupt demo, which didn't come with separate master/slave code so I assumed the demo would run on my board without any additional peripherals.&lt;/P&gt;&lt;P&gt;I'm new to embedded systems coding, any insight would be helpful.&lt;/P&gt;&lt;P&gt;Board is: MIMXRT1170-EVK&lt;/P&gt;&lt;P&gt;SDK is: SDK_2.x_MIMXRT1170-EVK (SDK Version 2.10.1)&lt;/P&gt;&lt;P&gt;Demo is: evkmimxrt1170_lpi2c_interrupt_cm7&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 17:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-demo/m-p/1374503#M183309</guid>
      <dc:creator>CMoran</dc:creator>
      <dc:date>2021-11-19T17:30:03Z</dc:date>
    </item>
    <item>
      <title>Re: I2C demo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-demo/m-p/1374695#M183342</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Before answering your question, I was wondering if you can share the printed result.&lt;BR /&gt;Further, I'd like to confirm that whether you set the MIMXRT1170-EVK as the readme.txt illustrates.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 22 Nov 2021 02:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-demo/m-p/1374695#M183342</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-11-22T02:47:28Z</dc:date>
    </item>
  </channel>
</rss>