<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8qxp - MIPI_CSI0_MCLK_OUT for camera clock?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1373014#M183176</link>
    <description>&lt;P&gt;Hi Dfdf&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to change status to "okay" as in example&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-ov5640.dtsi?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-ov5640.dtsi?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Thu, 18 Nov 2021 00:44:03 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-11-18T00:44:03Z</dc:date>
    <item>
      <title>imx8qxp - MIPI_CSI0_MCLK_OUT for camera clock?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1372761#M183153</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to clock my OV5640 through the MIPI_CSI0_MCLK_OUT pin. With the configuration below, there is no clock signal on this pin. Any idea why? Do I need to use a different clock source coming from the ACM module?&lt;/P&gt;&lt;P&gt;DT for Camera:&lt;/P&gt;&lt;P&gt;/* MIPI-CSI0 I2C available on MIPI Camera connector */&lt;/P&gt;&lt;P&gt;&amp;amp;i2c_mipi_csi0 {&lt;/P&gt;&lt;P&gt;#address-cells = &amp;lt;1&amp;gt;;&lt;/P&gt;&lt;P&gt;#size-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;pinctrl-names = "default", "gpio";&lt;/P&gt;&lt;P&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_csi0_lpi2c0&amp;gt;;&lt;/P&gt;&lt;P&gt;pinctrl-1 = &amp;lt;&amp;amp;pinctrl_csi0_lpi2c0_gpio&amp;gt;;&lt;/P&gt;&lt;P&gt;scl-gpios = &amp;lt;&amp;amp;lsio_gpio3 5 GPIO_ACTIVE_HIGH&amp;gt;;&lt;/P&gt;&lt;P&gt;sda-gpios = &amp;lt;&amp;amp;lsio_gpio3 6 GPIO_ACTIVE_HIGH&amp;gt;;&lt;/P&gt;&lt;P&gt;clock-frequency = &amp;lt;100000&amp;gt;;&lt;/P&gt;&lt;P&gt;status = "disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* MIPI-CSI2 camera */&lt;/P&gt;&lt;P&gt;ov5640_mipi: ov5640_mipi@3c {&lt;/P&gt;&lt;P&gt;compatible = "ovti,ov5640";&lt;/P&gt;&lt;P&gt;reg = &amp;lt;0x3c&amp;gt;;&lt;/P&gt;&lt;P&gt;pinctrl-names = "default";&lt;/P&gt;&lt;P&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_mipi&amp;gt;;&lt;/P&gt;&lt;P&gt;clocks = &amp;lt;&amp;amp;xtal24m&amp;gt;;&lt;/P&gt;&lt;P&gt;clock-names = "xclk";&lt;/P&gt;&lt;P&gt;csi_id = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;reset-gpios = &amp;lt;&amp;amp;lsio_gpio3 3 GPIO_ACTIVE_LOW&amp;gt;;&lt;/P&gt;&lt;P&gt;powerdown-gpios = &amp;lt;&amp;amp;lsio_gpio3 2 GPIO_ACTIVE_HIGH&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mclk = &amp;lt;24000000&amp;gt;;&lt;/P&gt;&lt;P&gt;mclk_source = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;mipi_csi;&lt;/P&gt;&lt;P&gt;status = "disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;port {&lt;/P&gt;&lt;P&gt;ov5640_mipi_ep: endpoint {&lt;/P&gt;&lt;P&gt;remote-endpoint = &amp;lt;&amp;amp;mipi_csi0_ep&amp;gt;;&lt;/P&gt;&lt;P&gt;data-lanes = &amp;lt;1 2&amp;gt;;&lt;/P&gt;&lt;P&gt;clocks-lanes = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DT for the clock (from freescale/imx8qxp)&lt;/P&gt;&lt;P&gt;xtal24m: clock-xtal24m {&lt;/P&gt;&lt;P&gt;compatible = "fixed-clock";&lt;/P&gt;&lt;P&gt;#clock-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;clock-frequency = &amp;lt;24000000&amp;gt;;&lt;/P&gt;&lt;P&gt;clock-output-names = "xtal_24MHz";&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mipi pinctrl:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;pinctrl_mipi: mipi {&lt;/P&gt;&lt;P&gt;fsl,pins = &amp;lt;&lt;/P&gt;&lt;P&gt;IMX8QXP_CSI_RESET_LSIO_GPIO3_IO03 0xC0000041&lt;/P&gt;&lt;P&gt;IMX8QXP_CSI_EN_LSIO_GPIO3_IO02 0xC0000041&lt;/P&gt;&lt;P&gt;IMX8QXP_MIPI_CSI0_MCLK_OUT_MIPI_CSI0_ACM_MCLK_OUT 0xc0000041&lt;/P&gt;&lt;P&gt;&amp;gt;;&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 12:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1372761#M183153</guid>
      <dc:creator>olliistmeinname</dc:creator>
      <dc:date>2021-11-17T12:52:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp - MIPI_CSI0_MCLK_OUT for camera clock?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1373014#M183176</link>
      <description>&lt;P&gt;Hi Dfdf&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to change status to "okay" as in example&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-ov5640.dtsi?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-ov5640.dtsi?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 18 Nov 2021 00:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1373014#M183176</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-18T00:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp - MIPI_CSI0_MCLK_OUT for camera clock?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1374583#M183319</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;That was is, now it works! So simple....&lt;/P&gt;&lt;P&gt;I would set the mipi and i2c status="okay" with an overlay, but for some reason it has to be done directly.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dfdf&lt;/P&gt;</description>
      <pubDate>Sat, 20 Nov 2021 00:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-MIPI-CSI0-MCLK-OUT-for-camera-clock/m-p/1374583#M183319</guid>
      <dc:creator>olliistmeinname</dc:creator>
      <dc:date>2021-11-20T00:56:23Z</dc:date>
    </item>
  </channel>
</rss>