<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFlash configuration for NXP i.MX8M Mini Cortex-M4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flash-configuration-for-NXP-i-MX8M-Mini-Cortex-M4/m-p/1372798#M183156</link>
    <description>&lt;P&gt;I am currently working on the Cortex-M4 processor of the NXP i.MX8M Mini.&lt;BR /&gt;I am able to load the M4 binary from U-boot via DDR and TCM.&lt;BR /&gt;I would like now to program the M4 via a JTAG probe.&lt;BR /&gt;So I have created a project on SEGGER J-Flash and I can connect via the probe.&lt;BR /&gt;However, I don't know what configuration to enter to flash the program.&lt;/P&gt;&lt;P&gt;Probe: SEGGER 5.07.01 Flasher ARM&lt;BR /&gt;Flashing software : SEGGER J-Flash V7.50&lt;BR /&gt;OS : Windows 10&lt;BR /&gt;Development board : i.MX 8M Mini EVK&lt;/P&gt;</description>
    <pubDate>Wed, 17 Nov 2021 13:32:26 GMT</pubDate>
    <dc:creator>martindenion</dc:creator>
    <dc:date>2021-11-17T13:32:26Z</dc:date>
    <item>
      <title>Flash configuration for NXP i.MX8M Mini Cortex-M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-configuration-for-NXP-i-MX8M-Mini-Cortex-M4/m-p/1372798#M183156</link>
      <description>&lt;P&gt;I am currently working on the Cortex-M4 processor of the NXP i.MX8M Mini.&lt;BR /&gt;I am able to load the M4 binary from U-boot via DDR and TCM.&lt;BR /&gt;I would like now to program the M4 via a JTAG probe.&lt;BR /&gt;So I have created a project on SEGGER J-Flash and I can connect via the probe.&lt;BR /&gt;However, I don't know what configuration to enter to flash the program.&lt;/P&gt;&lt;P&gt;Probe: SEGGER 5.07.01 Flasher ARM&lt;BR /&gt;Flashing software : SEGGER J-Flash V7.50&lt;BR /&gt;OS : Windows 10&lt;BR /&gt;Development board : i.MX 8M Mini EVK&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 13:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-configuration-for-NXP-i-MX8M-Mini-Cortex-M4/m-p/1372798#M183156</guid>
      <dc:creator>martindenion</dc:creator>
      <dc:date>2021-11-17T13:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flash configuration for NXP i.MX8M Mini Cortex-M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-configuration-for-NXP-i-MX8M-Mini-Cortex-M4/m-p/1372966#M183172</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may try as specified in the SDK documentation attached, chapter 5.1.3 Run an example application&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 20:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-configuration-for-NXP-i-MX8M-Mini-Cortex-M4/m-p/1372966#M183172</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-11-17T20:19:31Z</dc:date>
    </item>
  </channel>
</rss>