<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAAM: ICV error when loading back a black key in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAAM-ICV-error-when-loading-back-a-black-key/m-p/1371801#M183080</link>
    <description>&lt;P&gt;We are trying to use the CAAM on i.MX 8M Mini with black keys.&lt;/P&gt;&lt;P&gt;First we create a black key by running the following job descriptor.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;b081000d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;12820004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;00000020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;82500010&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;14810004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;00000020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;10880004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;e000006d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;64140020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b17000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a1001001&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;This job descriptor first generates 32 bytes of random data, then loads it into a key register and then uses the FIFO store to export the black key in AES-256-CCM. As far as we can tell, this works as expected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Then we want to encapsulate the black key into a blob using the following job descriptor:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;b0810008&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;f000002c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b17000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;f8000060&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b42000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;870d0104&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a1001001&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;The job descriptor uses the protocol operation command with the blob protocol to encapsulate, but it returns the status code&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;2000051a&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;Which according to the security reference manual designates an ICV error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;We cannot find any reason for this ICV error as we are using the freshly generated black key and loading it with the same parameters as it was exported (AES-256-CCM with JDKEK).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can anyone find our mistake?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Nov 2021 08:38:21 GMT</pubDate>
    <dc:creator>throwException</dc:creator>
    <dc:date>2021-11-16T08:38:21Z</dc:date>
    <item>
      <title>CAAM: ICV error when loading back a black key</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAAM-ICV-error-when-loading-back-a-black-key/m-p/1371801#M183080</link>
      <description>&lt;P&gt;We are trying to use the CAAM on i.MX 8M Mini with black keys.&lt;/P&gt;&lt;P&gt;First we create a black key by running the following job descriptor.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;b081000d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;12820004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;00000020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;82500010&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;14810004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;00000020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;10880004&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;e000006d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;64140020&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b17000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a1001001&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;This job descriptor first generates 32 bytes of random data, then loads it into a key register and then uses the FIFO store to export the black key in AES-256-CCM. As far as we can tell, this works as expected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Then we want to encapsulate the black key into a blob using the following job descriptor:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;b0810008&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;f000002c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b17000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;f8000060&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;43b42000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;870d0104&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a2000001&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;a1001001&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;The job descriptor uses the protocol operation command with the blob protocol to encapsulate, but it returns the status code&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;2000051a&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;Which according to the security reference manual designates an ICV error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;We cannot find any reason for this ICV error as we are using the freshly generated black key and loading it with the same parameters as it was exported (AES-256-CCM with JDKEK).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can anyone find our mistake?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 08:38:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAAM-ICV-error-when-loading-back-a-black-key/m-p/1371801#M183080</guid>
      <dc:creator>throwException</dc:creator>
      <dc:date>2021-11-16T08:38:21Z</dc:date>
    </item>
    <item>
      <title>Re: CAAM: ICV error when loading back a black key</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAAM-ICV-error-when-loading-back-a-black-key/m-p/1374215#M183284</link>
      <description>&lt;P&gt;For the record: The problem was the input length stated in the SEQ IN PTR command. This needs to be the length of the key (32 bytes) instead of the length of the black key data (32 + 12 bytes).&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 09:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAAM-ICV-error-when-loading-back-a-black-key/m-p/1374215#M183284</guid>
      <dc:creator>throwException</dc:creator>
      <dc:date>2021-11-19T09:10:59Z</dc:date>
    </item>
  </channel>
</rss>