<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 64-bit only Android for i.MX8 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1371792#M183079</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I found a user guide for 64 bit system&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Nov 2021 08:29:04 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2021-11-16T08:29:04Z</dc:date>
    <item>
      <title>64-bit only Android for i.MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1365196#M182499</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was wondering if NXP has all of the drivers, shared objects, and proprietary firmware necessary to support a 64-bit only build of Android on i.MX8?&lt;/P&gt;&lt;P&gt;I tried building a 64-bit only build of Android 9, but this failed due to the lack of 64-bit drivers for some of the VPU and media components. I didn't have enough time to investigate further.&lt;/P&gt;&lt;P&gt;I would like to know if this is possible, as 32-bit software is something we don't need to support and it would be nice to reduce the amount of legacy code in the system to a minimum. This also helps cut the AOSP build time almost in half, and reduces the size of the OTA update packages.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Max&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 13:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1365196#M182499</guid>
      <dc:creator>max-WL</dc:creator>
      <dc:date>2021-11-02T13:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: 64-bit only Android for i.MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1365548#M182537</link>
      <description>&lt;P&gt;As i kown, we don't have a plan to publish&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;64-bit drivers for some of the VPU and media components&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 07:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1365548#M182537</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-11-03T07:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: 64-bit only Android for i.MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1369214#M182852</link>
      <description>&lt;P&gt;Ahh, ok. It would be very nice to have a pure 64-bit system for simplicity and security purposes. The only reason we're keeping 32-bit around right now at all is because of the media components.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 10:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1369214#M182852</guid>
      <dc:creator>max-WL</dc:creator>
      <dc:date>2021-11-10T10:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: 64-bit only Android for i.MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1371792#M183079</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I found a user guide for 64 bit system&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 08:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1371792#M183079</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-11-16T08:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: 64-bit only Android for i.MX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1373439#M183221</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This helps with porting software and other existing resources to 64-bit, but doesn't help with the missing 64-bit firmware issue.&lt;/P&gt;&lt;P&gt;Has anyone at NXP attempted to build and run Android using &lt;A href="https://android.googlesource.com/platform/build/+/refs/heads/master/target/product/core_64_bit_only.mk" target="_self"&gt;build/make/target/product/core_64_bit_only.mk&lt;/A&gt;&amp;nbsp;in ProductConfigCommon.mk?&lt;/P&gt;&lt;P&gt;That would be a good starting point for building a 64-bit clean version.&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
      <pubDate>Thu, 18 Nov 2021 10:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/64-bit-only-Android-for-i-MX8/m-p/1373439#M183221</guid>
      <dc:creator>max-WL</dc:creator>
      <dc:date>2021-11-18T10:54:14Z</dc:date>
    </item>
  </channel>
</rss>