<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't debug iMX when input pin is high in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1371779#M183075</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;sorry for the delayed response and thanks for your help. It turned out that we had an unstable supply voltage at start-up which was obviously causing the issue. With the supply voltage fixed and stable the issue didn't occur anymore.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
    <pubDate>Tue, 16 Nov 2021 08:19:17 GMT</pubDate>
    <dc:creator>Michi_O</dc:creator>
    <dc:date>2021-11-16T08:19:17Z</dc:date>
    <item>
      <title>Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1354299#M181414</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have an issue with &lt;STRONG&gt;debugging&lt;/STRONG&gt; / accessing the controller with &lt;STRONG&gt;J-Link&lt;/STRONG&gt;. &lt;STRONG&gt;GPIO pins&lt;/STRONG&gt; are initially set as &lt;STRONG&gt;input&lt;/STRONG&gt; pins after a reset (corresponding registers default as 0). Whenever a high signal is applied to one of these GPIOs the J-Link probe &lt;STRONG&gt;fails to connect&lt;/STRONG&gt; to the target. In my specific case, one GPIO is later initialized as a CS for SPI communication (slave). Therefore, the device the iMX is communicating with is raising the signal before I can start the debugging process and the probe fails to connect via &lt;STRONG&gt;SWD&lt;/STRONG&gt;. If the CS line is cut I can debug as usual.&lt;/P&gt;&lt;P&gt;Is there a way around this behavior? Unfortunately there is no proper way in the given system to keep the CS line low when programming.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a &lt;STRONG&gt;MIMXRT1052DVL6B&lt;/STRONG&gt; and &lt;STRONG&gt;Segger J-Link&lt;/STRONG&gt; with &lt;STRONG&gt;MCUXpresso IDE&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 14:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1354299#M181414</guid>
      <dc:creator>Michi_O</dc:creator>
      <dc:date>2021-10-12T14:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1355724#M181546</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190368"&gt;@Michi_O&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Please tell me which detail pin you use will influence the debugger? Whether it is the JTAG_MOD pin or other SWD related pins?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1634201869301.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159110i8E4B86AF91CF3E74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1634201869301.png" alt="kerryzhou_0-1634201869301.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This pin needs to be low, otherwise, it will influence the debug mode.&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 08:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1355724#M181546</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-10-14T08:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1355882#M181563</link>
      <description>&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;thanks for your response. Additionally to my previous findings I figured out that not (only) a high signal on the observed pins is causing the connection issue. It also appears when a pin is simply connected to the rest of the system. Unfortunately, the behavior can't be determined by specific pins. It is completely random and may or may not occur when a certain pin is connected. However, when the controller board is connected to the system with all pins (LPSPI1 - LPSPI4, LPI2C1 and a few GPIOs) the debugger can never connect.&lt;/P&gt;&lt;P&gt;I could see that in such cases the SWDIO and SWDCLK lines change their initial level (sometimes high, sometimes low). I fixed this by applying pull-ups as stated by the table from your previous post. The JTAG_MOD pin was pulled-down by 100k which I also changed to 4.7k as stated in the table. Unfortunately, all measures were unsuccessful.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 13:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1355882#M181563</guid>
      <dc:creator>Michi_O</dc:creator>
      <dc:date>2021-10-14T13:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1356196#M181589</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190368"&gt;@Michi_O&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Can you do the same test on the NXP official MIMXRT1050-EVKB board? Whether you meet the same issues with your customer board or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Seems your hardware have the intereference signal, which influence the SWD. What about your PCB ground, whether it is influenced or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 05:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1356196#M181589</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-10-15T05:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1371779#M183075</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;sorry for the delayed response and thanks for your help. It turned out that we had an unstable supply voltage at start-up which was obviously causing the issue. With the supply voltage fixed and stable the issue didn't occur anymore.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 08:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1371779#M183075</guid>
      <dc:creator>Michi_O</dc:creator>
      <dc:date>2021-11-16T08:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug iMX when input pin is high</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1371784#M183076</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190368"&gt;@Michi_O&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Thanks for your information sharing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Next time, if you have any issues about the RT, please create the question post under this link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/bd-p/imxrt" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/bd-p/imxrt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 08:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-debug-iMX-when-input-pin-is-high/m-p/1371784#M183076</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-11-16T08:23:12Z</dc:date>
    </item>
  </channel>
</rss>