<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ull spi master could not read data from FRAM.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1368521#M182795</link>
    <description>&lt;P&gt;To make me able to accurately answer your question, please first specify what &lt;BR /&gt;exactly i.MX family processor do you use and what software runs on top of it. Is &lt;BR /&gt;it MCUXpresso SDK? If so, plesae specify the SDK version.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Tue, 09 Nov 2021 11:09:53 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2021-11-09T11:09:53Z</dc:date>
    <item>
      <title>imx6ull spi master could not read data from FRAM.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1364766#M182441</link>
      <description>&lt;P&gt;I use the spi master to read the data from the SPI slave FRAM mb85rs512t by the free rtos SDK non-blocking transfer. only one slave device was connected to the SPI interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;it contains the read command and some dummy data in a transfer. as the data sheet, the CS line should keep low during the whole operation and was set to automatic mode. and the spi was set to single burst and 8 bit as the burst length.so basically the interrupt works well . However the read data is always 0.&lt;/P&gt;&lt;P&gt;But when I change it to the block mode , and set the CS manual mode.&amp;nbsp; or i use the loop back test to see the data, both of them work well.&lt;/P&gt;&lt;P&gt;So could anyone show me how to configure the CS pin automatic configuration ? or any other advice. was blocked here for several days.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 02:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1364766#M182441</guid>
      <dc:creator>alven</dc:creator>
      <dc:date>2021-11-02T02:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull spi master could not read data from FRAM.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1368521#M182795</link>
      <description>&lt;P&gt;To make me able to accurately answer your question, please first specify what &lt;BR /&gt;exactly i.MX family processor do you use and what software runs on top of it. Is &lt;BR /&gt;it MCUXpresso SDK? If so, plesae specify the SDK version.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 11:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1368521#M182795</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-11-09T11:09:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull spi master could not read data from FRAM.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1372012#M183092</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12421"&gt;@art&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi im also having the same problem not able to read data from sensor using MIMXRT1060 module. the sdk only having example to communicate between controllers not to connect with external sensors&amp;nbsp;&lt;/P&gt;&lt;P&gt;im using&amp;nbsp;SPI_EVKRT1060_lpspi_polling_b2b_transfer_master these examples&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 12:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-spi-master-could-not-read-data-from-FRAM/m-p/1372012#M183092</guid>
      <dc:creator>jinu_mohan</dc:creator>
      <dc:date>2021-11-16T12:46:36Z</dc:date>
    </item>
  </channel>
</rss>