<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMXRT106S|| Audio/ Speaker Connection/ Audio processing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1368462#M182790</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Are you recommending attached image for MQS driver circuitry?&lt;/P&gt;&lt;P&gt;Q1- In this circuitry, Is Power AMP required in between buffer and audio jack?&lt;/P&gt;&lt;P&gt;Q2- Attaching the image of our schematic dig for the implementation of speaker connection, Can you please confirm whether it will work or not? If any modification required, please comment.&lt;/P&gt;&lt;P&gt;Also please share the test code and drivers needed.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Nov 2021 09:45:35 GMT</pubDate>
    <dc:creator>goyal9076</dc:creator>
    <dc:date>2021-11-09T09:45:35Z</dc:date>
    <item>
      <title>MIMXRT106|| Audio/ Speaker Connection/ Audio processing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1364487#M182410</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing problem in interfacing speaker. Till now I have understand that MQS pin are used for that. Is there any other provision other than this?&lt;/P&gt;&lt;P&gt;Also need to have a block diagram for&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;audio&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;processing if I/P is provided at SAI3 pins through I2S communication.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 10:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1364487#M182410</guid>
      <dc:creator>goyal9076</dc:creator>
      <dc:date>2021-11-01T10:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106|| Audio/ Speaker Connection/ Audio processing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1366165#M182583</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well.&lt;BR /&gt;Yes, you can use the MQS to interface a speaker but you will need external circuitry since the output is a PWM signal.&lt;/P&gt;
&lt;P&gt;This post might be helpful since it refers to the circuit to connect the speaker as well as an example code: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can also connect a speaker through an external audio codec like WM8960 that is on our boards. The example codes can be found at the SDK. &lt;BR /&gt;&lt;BR /&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 04 Nov 2021 01:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1366165#M182583</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-11-04T01:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106S|| Audio/ Speaker Connection/ Audio processing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1368462#M182790</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Are you recommending attached image for MQS driver circuitry?&lt;/P&gt;&lt;P&gt;Q1- In this circuitry, Is Power AMP required in between buffer and audio jack?&lt;/P&gt;&lt;P&gt;Q2- Attaching the image of our schematic dig for the implementation of speaker connection, Can you please confirm whether it will work or not? If any modification required, please comment.&lt;/P&gt;&lt;P&gt;Also please share the test code and drivers needed.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 09:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1368462#M182790</guid>
      <dc:creator>goyal9076</dc:creator>
      <dc:date>2021-11-09T09:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106S|| Audio/ Speaker Connection/ Audio processing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1370879#M182991</link>
      <description>&lt;P&gt;Yes, the circuit attached from my colleague can be helpful. With the 74vc244 you won´t need an RC circuit.&lt;/P&gt;
&lt;P&gt;A1 - No, the parts in that circuitry are enough to reproduce music.&lt;/P&gt;
&lt;P&gt;A2 - Your schematic looks fine. We have to consider that the output from MQS is a PWM signal so we first need to add an RC filter and improve the signal with an amplifier. &lt;BR /&gt;The example was uploaded by Kerry in this post:&amp;nbsp; &lt;A href="https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070&lt;/A&gt;&lt;BR /&gt;For the drivers you need to install the SDK: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Sat, 13 Nov 2021 03:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-Audio-Speaker-Connection-Audio-processing/m-p/1370879#M182991</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-11-13T03:27:56Z</dc:date>
    </item>
  </channel>
</rss>