<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MN UART1 can not receive data in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1368272#M182774</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;			uart1: serial@30860000 {
				compatible = "fsl,imx8mn-uart", "fsl,imx6q-uart";
				reg = &amp;lt;0x30860000 0x10000&amp;gt;;
				interrupts = &amp;lt;GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
				clocks = &amp;lt;&amp;amp;clk IMX8MN_CLK_UART1_ROOT&amp;gt;,
					 &amp;lt;&amp;amp;clk IMX8MN_CLK_UART1_ROOT&amp;gt;;
				clock-names = "ipg", "per";
				dmas = &amp;lt;&amp;amp;sdma1 22 4 0&amp;gt;, &amp;lt;&amp;amp;sdma1 23 4 0&amp;gt;;
				dma-names = "rx", "tx";
				status = "disabled";
			};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;sdma.bin is not integrated in rootFS.&lt;/SPAN&gt;&lt;SPAN class=""&gt;UART1 depends on SDMA. So t&lt;/SPAN&gt;&lt;SPAN class=""&gt;he UART1 function is abnormal&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 09 Nov 2021 07:03:08 GMT</pubDate>
    <dc:creator>link</dc:creator>
    <dc:date>2021-11-09T07:03:08Z</dc:date>
    <item>
      <title>IMX8MN UART1 can not receive data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1365119#M182493</link>
      <description>&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Now we use UART1 of IMX8MN to communicate with PC. The device can send data, but cannot receive data. The correct waveform can be measured at the RX end of the device. It is OK to send and receive data in the same program on UART2.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; To confirm the question, use imx8mnevk as a comparison. we run unit_tests to text /dev/ttymxc0.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2021-11-02_19-38-41.bmp" style="width: 546px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160952i81C27B9AE8E39BFB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Snipaste_2021-11-02_19-38-41.bmp" alt="Snipaste_2021-11-02_19-38-41.bmp" /&gt;&lt;/span&gt;&lt;BR /&gt;For mxc_uart_test.out:&lt;BR /&gt;write and read data are OK&lt;/P&gt;&lt;LI-CODE lang="c"&gt;---- Running &amp;lt; ./mxc_uart_test.out &amp;gt; test ----

/dev/ttymxc0 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test

----  Test &amp;lt; /dev/ttymxc0 &amp;gt; ended  ----&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;For mxc_uart_stress_test.out&lt;BR /&gt;write data is OK, but tne receive data is empty.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="clipboard.png" style="width: 579px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160951iDCBFBB7ADA9EC00E/image-size/large?v=v2&amp;amp;px=999" role="button" title="clipboard.png" alt="clipboard.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;What may the cause? Does UART1 need additional software configuration for serial port&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 11:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1365119#M182493</guid>
      <dc:creator>link</dc:creator>
      <dc:date>2021-11-02T11:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MN UART1 can not receive data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1365370#M182509</link>
      <description>&lt;P&gt;Hi Yanlin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;may be recommended to check if signal present on uart1 pad with oscilloscope,&lt;/P&gt;
&lt;P&gt;for software check if IOMUXC_UART1_RX_SELECT_INPUT configured properly, it is described in&lt;/P&gt;
&lt;P&gt;sect.8.2.5.261 Select Input Register (IOMUXC_UART1_RX_SELECT_INPUT)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8MNRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Nano Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 00:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1365370#M182509</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-03T00:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MN UART1 can not receive data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1368272#M182774</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;			uart1: serial@30860000 {
				compatible = "fsl,imx8mn-uart", "fsl,imx6q-uart";
				reg = &amp;lt;0x30860000 0x10000&amp;gt;;
				interrupts = &amp;lt;GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
				clocks = &amp;lt;&amp;amp;clk IMX8MN_CLK_UART1_ROOT&amp;gt;,
					 &amp;lt;&amp;amp;clk IMX8MN_CLK_UART1_ROOT&amp;gt;;
				clock-names = "ipg", "per";
				dmas = &amp;lt;&amp;amp;sdma1 22 4 0&amp;gt;, &amp;lt;&amp;amp;sdma1 23 4 0&amp;gt;;
				dma-names = "rx", "tx";
				status = "disabled";
			};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;sdma.bin is not integrated in rootFS.&lt;/SPAN&gt;&lt;SPAN class=""&gt;UART1 depends on SDMA. So t&lt;/SPAN&gt;&lt;SPAN class=""&gt;he UART1 function is abnormal&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 07:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-UART1-can-not-receive-data/m-p/1368272#M182774</guid>
      <dc:creator>link</dc:creator>
      <dc:date>2021-11-09T07:03:08Z</dc:date>
    </item>
  </channel>
</rss>