<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Warning HAB event in U-Boot 2020.04 for i.MX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1367731#M182739</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We have a custom board with i.MX6Q rev 1.6.&lt;/P&gt;&lt;P&gt;Previously we were using the U-Boot 2017.03 which was from NXP BSP version fsl-yocto-L4.9.11_1.0.0.&lt;/P&gt;&lt;P&gt;With&amp;nbsp;U-Boot 2017.03, the following message were shown:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;Noted that&lt;/P&gt;&lt;P&gt;1) no message ""No HAB Events Found!" was displayed for this version.&lt;/P&gt;&lt;P&gt;2) the device can boot properly after closing it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently we are porting to the latest NXP BSP version&amp;nbsp;LF5.10.9_1.0.0. Now the U-Boot version is 2020.04.&lt;/P&gt;&lt;P&gt;With U-Boot 2020.04, we noticed the following HAB events:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x69 0x30 0xe1 0x1d&lt;BR /&gt;0x00 0x04 0x00 0x02 0x40 0x00 0x36 0x06&lt;BR /&gt;0x55 0x55 0x00 0x03 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;STS = HAB_WARNING (0x69)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_CAAM (0x1D)&lt;/P&gt;&lt;P&gt;Any idea what could be the problem? How to resolve it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it safe to close the device with this warning event?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional information:&lt;/P&gt;&lt;P&gt;We have one unit with the&amp;nbsp;i.MX6Q rev 1.2.&lt;/P&gt;&lt;P&gt;Using the same signed u-boot image for 2020.04, the following message is observed:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;BR /&gt;No HAB Events Found!&lt;/P&gt;&lt;P&gt;Q: why is the HAB event different for i.MX6Q rev 1.2 and 1.6?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your kindly help or advice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Shunnian&lt;/P&gt;</description>
    <pubDate>Mon, 08 Nov 2021 07:26:41 GMT</pubDate>
    <dc:creator>shunnianzhai</dc:creator>
    <dc:date>2021-11-08T07:26:41Z</dc:date>
    <item>
      <title>Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1367731#M182739</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We have a custom board with i.MX6Q rev 1.6.&lt;/P&gt;&lt;P&gt;Previously we were using the U-Boot 2017.03 which was from NXP BSP version fsl-yocto-L4.9.11_1.0.0.&lt;/P&gt;&lt;P&gt;With&amp;nbsp;U-Boot 2017.03, the following message were shown:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;Noted that&lt;/P&gt;&lt;P&gt;1) no message ""No HAB Events Found!" was displayed for this version.&lt;/P&gt;&lt;P&gt;2) the device can boot properly after closing it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently we are porting to the latest NXP BSP version&amp;nbsp;LF5.10.9_1.0.0. Now the U-Boot version is 2020.04.&lt;/P&gt;&lt;P&gt;With U-Boot 2020.04, we noticed the following HAB events:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x69 0x30 0xe1 0x1d&lt;BR /&gt;0x00 0x04 0x00 0x02 0x40 0x00 0x36 0x06&lt;BR /&gt;0x55 0x55 0x00 0x03 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;STS = HAB_WARNING (0x69)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_CAAM (0x1D)&lt;/P&gt;&lt;P&gt;Any idea what could be the problem? How to resolve it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it safe to close the device with this warning event?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional information:&lt;/P&gt;&lt;P&gt;We have one unit with the&amp;nbsp;i.MX6Q rev 1.2.&lt;/P&gt;&lt;P&gt;Using the same signed u-boot image for 2020.04, the following message is observed:&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;BR /&gt;No HAB Events Found!&lt;/P&gt;&lt;P&gt;Q: why is the HAB event different for i.MX6Q rev 1.2 and 1.6?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your kindly help or advice.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Shunnian&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 07:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1367731#M182739</guid>
      <dc:creator>shunnianzhai</dc:creator>
      <dc:date>2021-11-08T07:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1367832#M182748</link>
      <description>&lt;P&gt;Hi Shunnian&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Q: why is the HAB event different for i.MX6Q rev 1.2 and 1.6?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;those warnings are caused by RNG self test errors on some i.MX device revisions,&lt;/P&gt;
&lt;P&gt;for i.MX6Q only rev.1.6 is affected (additional details were sent via mail).&lt;/P&gt;
&lt;P&gt;Recommended to apply patch:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://portland.source.codeaurora.org/patches/external/imxsupport/uboot-imx/imx_v2016.03_4.1.15_2.0.0_ga/HAB-238-Run-RNG-self-test-for-impacted-i.MX-chips.zip" target="_blank"&gt;https://portland.source.codeaurora.org/patches/external/imxsupport/uboot-imx/imx_v2016.03_4.1.15_2.0.0_ga/HAB-238-Run-RNG-self-test-for-impacted-i.MX-chips.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 09:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1367832#M182748</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-08T09:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368207#M182772</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi Igor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks for your quick response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I will try to apply the patch and verify the fixing. Once done, I will update you on the result.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Noted that the patch &amp;nbsp;is only applicable to imx_v2016.03_4.1.15_2.0.0_ga branch of u-boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Is there any plan to apply the patch to the mainstream of the latest u-boot release so the issue can be completed resolved for future version?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Shunnian&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 05:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368207#M182772</guid>
      <dc:creator>shunnianzhai</dc:creator>
      <dc:date>2021-11-09T05:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368283#M182776</link>
      <description>&lt;P&gt;&amp;gt;&lt;SPAN class=""&gt;Is there any plan to apply the patch to the mainstream of the latest u-boot release so &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&amp;gt;the issue can be completed resolved for future version?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;no such plans, sorry.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;BR /&gt;igor&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 07:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368283#M182776</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-09T07:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368305#M182779</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Today I have tried to apply the patch to the u-boot code.&lt;/P&gt;&lt;P&gt;Also, add the following config into my defconfig file:&lt;/P&gt;&lt;P&gt;CONFIG_CMD_RNG_SELF_TEST=y&lt;/P&gt;&lt;P&gt;However, after I re-build the u-boot, I noted that&amp;nbsp;CONFIG_CMD_RNG_SELF_TEST is not included in the auto-generated file ".config".&lt;/P&gt;&lt;P&gt;So, when I do test, the issue is still existed.&lt;/P&gt;&lt;P&gt;Pls advice on how to add and ensure this config in the file ".config"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for your help,&lt;/P&gt;&lt;P&gt;Shunnian&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 07:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368305#M182779</guid>
      <dc:creator>shunnianzhai</dc:creator>
      <dc:date>2021-11-09T07:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368343#M182782</link>
      <description>&lt;P&gt;&amp;gt;Pls advice on how to add and ensure this config in the file ".config"?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I sent additional materials via mail, had you checked them ?&lt;/P&gt;
&lt;P&gt;In general, nxp has special service for helping with porting and applying patches:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://contact.nxp.com/new-prof-svcs-sw-tech" target="_blank"&gt;https://contact.nxp.com/new-prof-svcs-sw-tech&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 08:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1368343#M182782</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-09T08:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1369049#M182841</link>
      <description>&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;Yes, I read the additional materials you sent to me and do what need to do per doc carefully.&lt;/P&gt;&lt;P&gt;Since the patch is for u-Boot 2016.03, there are needs to change some files location when porting to U-Boot 2020.04. Also, need to change some header files name to fix the compile errors.&lt;/P&gt;&lt;P&gt;Now I managed to successfully build the following 2 newly-added files:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;cmd_rng_self_test.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;rng_self_test.c&lt;/P&gt;&lt;P&gt;However, when I test with the new u-boot image, it seems that the command "rng_self_test" is not recognized as the error shown below:&lt;/P&gt;&lt;P&gt;&amp;nbsp; =&amp;gt; rng_self_test&lt;BR /&gt;&amp;nbsp; Unknown command 'rng_self_test' - try 'help'&lt;/P&gt;&lt;P&gt;Please advise what could be wrong?&lt;/P&gt;&lt;P&gt;In addition, please advise if it is safe to close the device even if the following warning event is occurred? What is the best approach to resolve this issue?&lt;/P&gt;&lt;P&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x69 0x30 0xe1 0x1d&lt;BR /&gt;0x00 0x04 0x00 0x02 0x40 0x00 0x36 0x06&lt;BR /&gt;0x55 0x55 0x00 0x03 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;STS = HAB_WARNING (0x69)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_CAAM (0x1D)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Shunnian&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 07:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1369049#M182841</guid>
      <dc:creator>shunnianzhai</dc:creator>
      <dc:date>2021-11-10T07:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: Warning HAB event in U-Boot 2020.04 for i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1369191#M182849</link>
      <description>&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;Some good progress today.&lt;/P&gt;&lt;P&gt;I managed to run command "rng_self_test" successfully.&lt;/P&gt;&lt;P&gt;However, it shows some errors as below. Pls advise on what I should do next. What could be the issue?&lt;/P&gt;&lt;P&gt;=&amp;gt; rng_self_test 10000000&lt;BR /&gt;RNG SELF TEST DESCRIPTOR:&lt;BR /&gt;0xB0800036&lt;BR /&gt;0x04800010&lt;BR /&gt;0x3C85A15B&lt;BR /&gt;0x50A9D0B1&lt;BR /&gt;0x71A09FEE&lt;BR /&gt;0x2EECF20B&lt;BR /&gt;0x02800020&lt;BR /&gt;0xB267292E&lt;BR /&gt;0x85BF712D&lt;BR /&gt;0xE85FF43A&lt;BR /&gt;0xA716B7FB&lt;BR /&gt;0xC40BB528&lt;BR /&gt;0x27B6F564&lt;BR /&gt;0x8821CB5D&lt;BR /&gt;0x9B5F6C26&lt;BR /&gt;0x12A00020&lt;BR /&gt;0x0A20DE17&lt;BR /&gt;0x6529357E&lt;BR /&gt;0x316277AB&lt;BR /&gt;0x2846254E&lt;BR /&gt;0x34D23BA5&lt;BR /&gt;0x6F5E9C32&lt;BR /&gt;0x7ABDC1BB&lt;BR /&gt;0x0197A385&lt;BR /&gt;0x82500405&lt;BR /&gt;0xA2000001&lt;BR /&gt;0x10880004&lt;BR /&gt;0x00000005&lt;BR /&gt;0x12820004&lt;BR /&gt;0x00000020&lt;BR /&gt;0x82500001&lt;BR /&gt;0xA2000001&lt;BR /&gt;0x10880004&lt;BR /&gt;0x40000045&lt;BR /&gt;0x02800020&lt;BR /&gt;0x8F389CC7&lt;BR /&gt;0xE7F7CBB0&lt;BR /&gt;0x6BF2073D&lt;BR /&gt;0xFC380B6D&lt;BR /&gt;0xB22E9D1A&lt;BR /&gt;0xEE64FCB7&lt;BR /&gt;0xA2B48D49&lt;BR /&gt;0xDF9BC3A4&lt;BR /&gt;0x82500009&lt;BR /&gt;0xA2000001&lt;BR /&gt;0x10880004&lt;BR /&gt;0x00000005&lt;BR /&gt;0x82500001&lt;BR /&gt;0x60340020&lt;BR /&gt;0x10000000&lt;BR /&gt;0xA2000001&lt;BR /&gt;0x10880004&lt;BR /&gt;0x00000005&lt;BR /&gt;0x8250000D&lt;/P&gt;&lt;P&gt;Error while running RNG self-test descriptor: 536877395&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;=&amp;gt; hab_status&lt;/P&gt;&lt;P&gt;Secure boot disabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xf0, HAB State: 0x66&lt;/P&gt;&lt;P&gt;--------- HAB Event 1 -----------------&lt;BR /&gt;event data:&lt;BR /&gt;0xdb 0x00 0x24 0x42 0x69 0x30 0xe1 0x1d&lt;BR /&gt;0x00 0x04 0x00 0x02 0x40 0x00 0x36 0x06&lt;BR /&gt;0x55 0x55 0x00 0x03 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00&lt;BR /&gt;0x00 0x00 0x00 0x01&lt;/P&gt;&lt;P&gt;STS = HAB_WARNING (0x69)&lt;BR /&gt;RSN = HAB_ENG_FAIL (0x30)&lt;BR /&gt;CTX = HAB_CTX_ENTRY (0xE1)&lt;BR /&gt;ENG = HAB_ENG_CAAM (0x1D)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Shunnian&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 09:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Warning-HAB-event-in-U-Boot-2020-04-for-i-MX6Q/m-p/1369191#M182849</guid>
      <dc:creator>shunnianzhai</dc:creator>
      <dc:date>2021-11-10T09:53:51Z</dc:date>
    </item>
  </channel>
</rss>