<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR Stress Test failed for IMX8DX Custom Board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367095#M182665</link>
    <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have used the latest scfw1.7.0 and MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16.xls。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Nov 2021 05:41:57 GMT</pubDate>
    <dc:creator>songhongliang</dc:creator>
    <dc:date>2021-11-05T05:41:57Z</dc:date>
    <item>
      <title>DDR Stress Test failed for IMX8DX Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367047#M182658</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;hi&amp;nbsp; nxp&lt;/P&gt;&lt;P&gt;my board cpu is imd8dx 16bit LPDDR4，please the fail, Can you provide me with some help to fix the error。&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test Version: ER14&lt;BR /&gt;Built on Mar 27 2020 12:28:23&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A35 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x13d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x101122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM Clock(CA35): 1200MHz&lt;BR /&gt;DDR Clock: 1200MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is LPDDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;Row size: 16, col size: 10&lt;BR /&gt;One chip select is used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;Density per controller is: 1024MB&lt;BR /&gt;Total density detected on the board is: 1024MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;********************************************&lt;BR /&gt;WARNING! DDR training errors were detected on DDRC 0!&lt;BR /&gt;DDR_PHY_PGSR0 = 0x806cc07f&lt;BR /&gt;DQS Gate training error detected&lt;BR /&gt;Write Leveling training error detected&lt;BR /&gt;VREF training error detected&lt;BR /&gt;Write DQS2DQ training error detected&lt;BR /&gt;Recheck DDR initialization&lt;BR /&gt;********************************************&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8QXP: Cortex-A35 is found&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 03:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367047#M182658</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2021-11-05T03:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test failed for IMX8DX Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367072#M182661</link>
      <description>&lt;P&gt;Hi Hongliang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;since all trainings are with errors, one can check with oscilloscope if there are any signals&lt;/P&gt;
&lt;P&gt;on memory. Also recommended to use latest MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16.xlsx on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 04:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367072#M182661</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-05T04:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test failed for IMX8DX Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367095#M182665</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have used the latest scfw1.7.0 and MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v16.xls。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 05:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367095#M182665</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2021-11-05T05:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test failed for IMX8DX Custom Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367131#M182671</link>
      <description>&lt;P&gt;&amp;gt;I have used the latest scfw1.7.0..&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;it is not latest, latest is v1.10.0&amp;nbsp; &lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/webapp/Download?colCode=L5.10.52_2.1.0_SCFWKIT-1.10.0&amp;amp;appType=license" target="_blank"&gt;SCFW Porting Kit​ 1.10.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 07:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-failed-for-IMX8DX-Custom-Board/m-p/1367131#M182671</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-11-05T07:01:23Z</dc:date>
    </item>
  </channel>
</rss>