<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGPU State Dump on imx8m plus with Android11 (2.2.0)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPU-State-Dump-on-imx8m-plus-with-Android11-2-2-0/m-p/1363490#M182277</link>
    <description>&lt;P&gt;I've been developing a system based on the i.mx8m plus with Android 11 1.2.0. &amp;nbsp;Recently, when upgrading &amp;nbsp;to the 2.2.0 branch, I've come across this issue:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.635706] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12
[   35.425694] GPU[1](ChipModel=0x8000 ChipRevision=0x8002):
[   35.431778] **************************
[   35.435559] ***   GPU STATE DUMP   ***
[   35.439334] **************************
[   35.443109]   axi      = 0x000000FF
[   35.446624]   idle     = 0x7FFFFFF7
[   35.450142]     SH not idle
[   35.452972]   DMA appears to be stuck at this address:
[   35.458138]     0xA4205B90
[   35.460868]   dmaLow   = 0x10000000
[   35.464381]   dmaHigh  = 0x00000000
[   35.467887]   dmaState = 0x00000000
[   35.471404]     command state       = 0 (PAR_IDLE_ST)&lt;/LI-CODE&gt;&lt;P&gt;The kernel pauses after a couple seconds of booting and prints nothing until this state dump. &amp;nbsp;It then immediately pauses again for another 30 seconds approx and prints another state dump. &amp;nbsp;After the 2nd dump, the system then boots up normally. &amp;nbsp;The dispay works and we can use the system as expected. &amp;nbsp;We need to solve the state dump and pausing during boot though.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestion where to debug to find out why this is occurring? &amp;nbsp;This only occurs on the Android 11 2.2.0 base and I've not seen it with any previous kernels.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Oct 2021 21:18:35 GMT</pubDate>
    <dc:creator>dennis3</dc:creator>
    <dc:date>2021-10-28T21:18:35Z</dc:date>
    <item>
      <title>GPU State Dump on imx8m plus with Android11 (2.2.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-State-Dump-on-imx8m-plus-with-Android11-2-2-0/m-p/1363490#M182277</link>
      <description>&lt;P&gt;I've been developing a system based on the i.mx8m plus with Android 11 1.2.0. &amp;nbsp;Recently, when upgrading &amp;nbsp;to the 2.2.0 branch, I've come across this issue:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.635706] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12
[   35.425694] GPU[1](ChipModel=0x8000 ChipRevision=0x8002):
[   35.431778] **************************
[   35.435559] ***   GPU STATE DUMP   ***
[   35.439334] **************************
[   35.443109]   axi      = 0x000000FF
[   35.446624]   idle     = 0x7FFFFFF7
[   35.450142]     SH not idle
[   35.452972]   DMA appears to be stuck at this address:
[   35.458138]     0xA4205B90
[   35.460868]   dmaLow   = 0x10000000
[   35.464381]   dmaHigh  = 0x00000000
[   35.467887]   dmaState = 0x00000000
[   35.471404]     command state       = 0 (PAR_IDLE_ST)&lt;/LI-CODE&gt;&lt;P&gt;The kernel pauses after a couple seconds of booting and prints nothing until this state dump. &amp;nbsp;It then immediately pauses again for another 30 seconds approx and prints another state dump. &amp;nbsp;After the 2nd dump, the system then boots up normally. &amp;nbsp;The dispay works and we can use the system as expected. &amp;nbsp;We need to solve the state dump and pausing during boot though.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestion where to debug to find out why this is occurring? &amp;nbsp;This only occurs on the Android 11 2.2.0 base and I've not seen it with any previous kernels.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 21:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-State-Dump-on-imx8m-plus-with-Android11-2-2-0/m-p/1363490#M182277</guid>
      <dc:creator>dennis3</dc:creator>
      <dc:date>2021-10-28T21:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: GPU State Dump on imx8m plus with Android11 (2.2.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-State-Dump-on-imx8m-plus-with-Android11-2-2-0/m-p/1363563#M182294</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167845"&gt;@dennis3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you also try android11(2.4.0)?&lt;/P&gt;</description>
      <pubDate>Fri, 29 Oct 2021 02:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-State-Dump-on-imx8m-plus-with-Android11-2-2-0/m-p/1363563#M182294</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-10-29T02:04:52Z</dc:date>
    </item>
  </channel>
</rss>