<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックstart kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/start-kernel/m-p/1362959#M182244</link>
    <description>&lt;P&gt;I currently have two base boards, one of them is working, we call it board A for the sake of description, and the other one is under debugging, we call it board B. Now I burned the kernel into IMX6U normally on board A, and it also boots normally.But when I put the IMX6U in the B board, it keeps printing the following message and can't enter the system, can you tell me what causes it?&lt;/P&gt;&lt;P&gt;[ 4.973429] ERROR: v4l2 capture: slave not found!&lt;BR /&gt;[ 4.978200] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 17.564390] usb 1-1: new high-speed USB device number 4 using ci_hdrc&lt;BR /&gt;[ 17.570923] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 28.034347] usb 1-1: device not accepting address 4, error -110&lt;BR /&gt;[ 28.040359] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 28.164347] usb 1-1: new high-speed USB device number 5 using ci_hdrc&lt;BR /&gt;[ 28.170869] imx-uart 2020000.serial: Rx FIFO overrun&lt;/P&gt;</description>
    <pubDate>Thu, 28 Oct 2021 05:31:14 GMT</pubDate>
    <dc:creator>Brilliant</dc:creator>
    <dc:date>2021-10-28T05:31:14Z</dc:date>
    <item>
      <title>start kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/start-kernel/m-p/1362959#M182244</link>
      <description>&lt;P&gt;I currently have two base boards, one of them is working, we call it board A for the sake of description, and the other one is under debugging, we call it board B. Now I burned the kernel into IMX6U normally on board A, and it also boots normally.But when I put the IMX6U in the B board, it keeps printing the following message and can't enter the system, can you tell me what causes it?&lt;/P&gt;&lt;P&gt;[ 4.973429] ERROR: v4l2 capture: slave not found!&lt;BR /&gt;[ 4.978200] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 17.564390] usb 1-1: new high-speed USB device number 4 using ci_hdrc&lt;BR /&gt;[ 17.570923] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 28.034347] usb 1-1: device not accepting address 4, error -110&lt;BR /&gt;[ 28.040359] imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;[ 28.164347] usb 1-1: new high-speed USB device number 5 using ci_hdrc&lt;BR /&gt;[ 28.170869] imx-uart 2020000.serial: Rx FIFO overrun&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 05:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/start-kernel/m-p/1362959#M182244</guid>
      <dc:creator>Brilliant</dc:creator>
      <dc:date>2021-10-28T05:31:14Z</dc:date>
    </item>
  </channel>
</rss>