<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFlashing android using prebuild image imx 8M</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1361726#M182161</link>
    <description>&lt;P&gt;Trying to flash i.mx 8M plus with android demo binaries using uuu tool but getting a continuous error with the flashing script. (using Linux 20)&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.138-0-g051a8fe&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;BR /&gt;1:14 1/ 2 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f "uuu_imx_android_flash.sh"&lt;/P&gt;</description>
    <pubDate>Tue, 26 Oct 2021 13:49:25 GMT</pubDate>
    <dc:creator>mukrsh</dc:creator>
    <dc:date>2021-10-26T13:49:25Z</dc:date>
    <item>
      <title>Flashing android using prebuild image imx 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1361726#M182161</link>
      <description>&lt;P&gt;Trying to flash i.mx 8M plus with android demo binaries using uuu tool but getting a continuous error with the flashing script. (using Linux 20)&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.138-0-g051a8fe&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;BR /&gt;1:14 1/ 2 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f "uuu_imx_android_flash.sh"&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 13:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1361726#M182161</guid>
      <dc:creator>mukrsh</dc:creator>
      <dc:date>2021-10-26T13:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing android using prebuild image imx 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1362624#M182217</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I don’t know which command you have used for your test, but please try with the following:&lt;/P&gt;
&lt;P&gt;sudo ./uuu_imx_android_flash.sh -f imx8mp -a -e&lt;/P&gt;
&lt;P&gt;This will flash the slot a to the eMMC with default features enabled (uboot and vbmeta)&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 18:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1362624#M182217</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-10-27T18:13:20Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing android using prebuild image imx 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1362648#M182220</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;still getting the same error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;@build-machine:~/mike-space/android/aosp/nxp/android-11.0.0_2.2.0_image_8mpevk$&lt;/STRONG&gt; &lt;EM&gt;sudo ./uuu_imx_android_flash.sh -f imx8mp -a -e&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[sudo] password for mukesh: &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;This script is validated with uuu 1.4.139 version, it is recommended to align with this version.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;dtbo is supported&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;dual slot is supported&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;dynamic parttition is supported&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;vendor_boot parttition is supported&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash u-boot-imx8mp.imx to the partition of bootloader0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash partition-table.img to the partition of gpt&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash dtbo-imx8mp.img to the partition of dtbo_a&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash boot.img to the partition of boot_a&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash vendor_boot.img to the partition of vendor_boot_a&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash vbmeta-imx8mp.img to the partition of vbmeta_a&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;generate lines to flash super.img to the partition of super&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.138-0-g051a8fe&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Wait for Known USB Device Appear...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: fail open file: &amp;gt;/tmp/uuu.lst&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also tried to echo manually,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;build-machine:/tmp$&lt;/STRONG&gt; &lt;EM&gt;sudo echo uuu_version 1.4.139 &amp;gt; uuu.lst&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bash: uuu.lst: Permission denied&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 19:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1362648#M182220</guid>
      <dc:creator>mukrsh</dc:creator>
      <dc:date>2021-10-27T19:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing android using prebuild image imx 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1364052#M182345</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Please make sure that you have UUU tool in the environment variable PATH. For Linux the executable will be uuu, you may download it here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.4.165/uuu" target="_blank"&gt;https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.4.165/uuu&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Even for a quick test you may place this file in the same folder as the android script.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Oct 2021 19:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1364052#M182345</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-10-29T19:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing android using prebuild image imx 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1365782#M182562</link>
      <description>&lt;P&gt;little modification in the script and that worked&lt;/P&gt;&lt;LI-CODE lang="java"&gt;echo "uuu script generated, start to invoke uuu with the generated uuu script"
if [ ${daemon_mode} -eq 1 ]; then
    ./uuu -d /tmp/uuu.lst
else
    ./uuu /tmp/uuu.lst
fi&lt;/LI-CODE&gt;</description>
      <pubDate>Wed, 03 Nov 2021 14:19:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-android-using-prebuild-image-imx-8M/m-p/1365782#M182562</guid>
      <dc:creator>mukrsh</dc:creator>
      <dc:date>2021-11-03T14:19:45Z</dc:date>
    </item>
  </channel>
</rss>