<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLCD Display contrast/gamma adjustment</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Display-contrast-gamma-adjustment/m-p/1361692#M182158</link>
    <description>&lt;DIV&gt;We have a 7 inch LCD display connected to our SOC (IMX6) and a QTE-based application is running on it (No X Window system).&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Everything is fine but the LCD contrast is not that good. The colors need to be a little darker.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;we have tried adjusting gamma using&amp;nbsp;MXCFB_SET_GAMMA ioctl (the source code is attached) and were able to see some changes in the color. but the colors are distorted.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;How to properly adjust the gamma/contrast of an LCD screen?&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;any help is appreciated.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks in advance.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
    <pubDate>Tue, 26 Oct 2021 13:04:47 GMT</pubDate>
    <dc:creator>slimSHA</dc:creator>
    <dc:date>2021-10-26T13:04:47Z</dc:date>
    <item>
      <title>LCD Display contrast/gamma adjustment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Display-contrast-gamma-adjustment/m-p/1361692#M182158</link>
      <description>&lt;DIV&gt;We have a 7 inch LCD display connected to our SOC (IMX6) and a QTE-based application is running on it (No X Window system).&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Everything is fine but the LCD contrast is not that good. The colors need to be a little darker.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;we have tried adjusting gamma using&amp;nbsp;MXCFB_SET_GAMMA ioctl (the source code is attached) and were able to see some changes in the color. but the colors are distorted.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;How to properly adjust the gamma/contrast of an LCD screen?&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;any help is appreciated.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks in advance.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Tue, 26 Oct 2021 13:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-Display-contrast-gamma-adjustment/m-p/1361692#M182158</guid>
      <dc:creator>slimSHA</dc:creator>
      <dc:date>2021-10-26T13:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Display contrast/gamma adjustment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-Display-contrast-gamma-adjustment/m-p/1361947#M182171</link>
      <description>&lt;P&gt;Hi Thejas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;may be useful to look at unit test examples&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test?h=lf-5.10.52_2.1.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test?h=lf-5.10.52_2.1.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 00:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-Display-contrast-gamma-adjustment/m-p/1361947#M182171</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-27T00:16:15Z</dc:date>
    </item>
  </channel>
</rss>