<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB 3.0 Performance on i.MX 8M in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-0-Performance-on-i-MX-8M/m-p/1361401#M182125</link>
    <description>&lt;P&gt;Hi, NXP Support Team.&lt;/P&gt;&lt;P&gt;I have an i.MX 8MQ development board.&lt;BR /&gt;I bought a USB 3.0 external hard case and NVMe M.2 SSD to test the USB 3.0 speed.&lt;BR /&gt;&lt;FONT size="2"&gt;USB 3.0 External Hard Case: RevuAhn UX980&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;NVMe M.2 SSD: Samsung 970 EVO Plus M.2 NVMe SSD 250GB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;The speed of the purchased external hard drive was checked from the USB 3.1(USB 3.2 Gen 2) port on the desktop.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVMe.png" style="width: 482px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160148i30476AD83878CE5F/image-size/large?v=v2&amp;amp;px=999" role="button" title="NVMe.png" alt="NVMe.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I did a speed test of the USB 3.0 external hard drive on the i.MX 8M development board with the dd command.&lt;BR /&gt;But the speed came out lower than I expected. Since it is USB 3.0, I expected a speed close to 500 MB/s.&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="100%" height="1873px"&gt;root@imx8mqevk:~# &lt;STRONG&gt;uname -a&lt;/STRONG&gt;&lt;BR /&gt;Linux imx8mqevk 5.4.70 #49 SMP PREEMPT Tue Oct 26 15:28:23 KST 2021 aarch64 aarch64 aarch64 GNU/Linux&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;[ 80.213250] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd&lt;BR /&gt;[ 80.246101] scsi host0: uas&lt;BR /&gt;[ 80.249722] scsi 0:0:0:0: Direct-Access RevuAhn UX980 0208 PQ: 0 ANSI: 6&lt;BR /&gt;[ 82.232773] sd 0:0:0:0: [sda] 488397168 512-byte logical blocks: (250 GB/233 GiB)&lt;BR /&gt;[ 82.240303] sd 0:0:0:0: [sda] 4096-byte physical blocks&lt;BR /&gt;[ 82.246092] sd 0:0:0:0: [sda] Write Protect is off&lt;BR /&gt;[ 82.251552] sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA&lt;BR /&gt;[ 82.261282] sd 0:0:0:0: [sda] Optimal transfer size 33553920 bytes not a multiple of physical block size (4096 bytes)&lt;BR /&gt;[ 82.296370] sda: sda1&lt;BR /&gt;[ 82.300315] sd 0:0:0:0: [sda] Attached SCSI disk&lt;BR /&gt;[ 82.598946] EXT4-fs (sda1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;df -h&lt;/STRONG&gt;&lt;BR /&gt;Filesystem Size Used Avail Use% Mounted on&lt;BR /&gt;/dev/root 5.5G 3.4G 1.8G 66% /&lt;BR /&gt;devtmpfs 994M 4.0K 994M 1% /dev&lt;BR /&gt;tmpfs 1.5G 0 1.5G 0% /dev/shm&lt;BR /&gt;tmpfs 1.5G 9.0M 1.5G 1% /run&lt;BR /&gt;tmpfs 1.5G 0 1.5G 0% /sys/fs/cgroup&lt;BR /&gt;tmpfs 1.5G 4.0K 1.5G 1% /tmp&lt;BR /&gt;tmpfs 1.5G 188K 1.5G 1% /var/volatile&lt;BR /&gt;/dev/mmcblk0p1 84M 30M 54M 36% /run/media/mmcblk0p1&lt;BR /&gt;/dev/mmcblk0p2 5.5G 3.9G 1.4G 75% /run/media/mmcblk0p2&lt;BR /&gt;/dev/mmcblk1p1 84M 30M 54M 36% /run/media/mmcblk1p1&lt;BR /&gt;tmpfs 296M 8.0K 296M 1% /run/user/0&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;/dev/sda1 230G 4.1G 214G 2% /run/media/sda1&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;mount&lt;/STRONG&gt;&lt;BR /&gt;/dev/mmcblk1p2 on / type ext4 (rw,relatime)&lt;BR /&gt;devtmpfs on /dev type devtmpfs (rw,relatime,size=1017540k,nr_inodes=254385,mode=755)&lt;BR /&gt;sysfs on /sys type sysfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;proc on /proc type proc (rw,relatime)&lt;BR /&gt;securityfs on /sys/kernel/security type securityfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /dev/shm type tmpfs (rw,nosuid,nodev)&lt;BR /&gt;devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620,ptmxmode=000)&lt;BR /&gt;tmpfs on /run type tmpfs (rw,nosuid,nodev,mode=755)&lt;BR /&gt;tmpfs on /sys/fs/cgroup type tmpfs (ro,nosuid,nodev,noexec,mode=755)&lt;BR /&gt;cgroup2 on /sys/fs/cgroup/unified type cgroup2 (rw,nosuid,nodev,noexec,relatime,nsdelegate)&lt;BR /&gt;cgroup on /sys/fs/cgroup/systemd type cgroup (rw,nosuid,nodev,noexec,relatime,xattr,name=systemd)&lt;BR /&gt;pstore on /sys/fs/pstore type pstore (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;cgroup on /sys/fs/cgroup/hugetlb type cgroup (rw,nosuid,nodev,noexec,relatime,hugetlb)&lt;BR /&gt;cgroup on /sys/fs/cgroup/cpu,cpuacct type cgroup (rw,nosuid,nodev,noexec,relatime,cpu,cpuacct)&lt;BR /&gt;cgroup on /sys/fs/cgroup/pids type cgroup (rw,nosuid,nodev,noexec,relatime,pids)&lt;BR /&gt;cgroup on /sys/fs/cgroup/blkio type cgroup (rw,nosuid,nodev,noexec,relatime,blkio)&lt;BR /&gt;cgroup on /sys/fs/cgroup/cpuset type cgroup (rw,nosuid,nodev,noexec,relatime,cpuset)&lt;BR /&gt;cgroup on /sys/fs/cgroup/memory type cgroup (rw,nosuid,nodev,noexec,relatime,memory)&lt;BR /&gt;cgroup on /sys/fs/cgroup/devices type cgroup (rw,nosuid,nodev,noexec,relatime,devices)&lt;BR /&gt;cgroup on /sys/fs/cgroup/perf_event type cgroup (rw,nosuid,nodev,noexec,relatime,perf_event)&lt;BR /&gt;hugetlbfs on /dev/hugepages type hugetlbfs (rw,relatime,pagesize=2M)&lt;BR /&gt;mqueue on /dev/mqueue type mqueue (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;debugfs on /sys/kernel/debug type debugfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /tmp type tmpfs (rw,nosuid,nodev)&lt;BR /&gt;configfs on /sys/kernel/config type configfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /var/volatile type tmpfs (rw,relatime)&lt;BR /&gt;/dev/mmcblk0p1 on /run/media/mmcblk0p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;BR /&gt;/dev/mmcblk0p2 on /run/media/mmcblk0p2 type ext4 (rw,relatime)&lt;BR /&gt;/dev/mmcblk1p1 on /run/media/mmcblk1p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;BR /&gt;tmpfs on /run/user/0 type tmpfs (rw,nosuid,nodev,relatime,size=302092k,mode=700)&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;/dev/sda1 on /run/media/sda1 type ext4 (rw,relatime)&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;echo 3 &amp;gt; /proc/sys/vm/drop_caches&lt;/STRONG&gt;&lt;BR /&gt;[ 182.039954] sh (632): drop_caches: 3&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;sync ; dd if=/dev/zero of=/run/media/sda1/largefile bs=1G count=4 oflag=direct ; sync&lt;/STRONG&gt;&lt;BR /&gt;4+0 records in&lt;BR /&gt;4+0 records out&lt;BR /&gt;4294967296 bytes (4.3 GB, 4.0 GiB) copied, 12.2417 s, &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;351 MB/s&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;sync ; dd if=/run/media/sda1/largefile of=/dev/null bs=1G count=4 ; sync&lt;/STRONG&gt;&lt;BR /&gt;4+0 records in&lt;BR /&gt;4+0 records out&lt;BR /&gt;4294967296 bytes (4.3 GB, 4.0 GiB) copied, 11.7799 s, &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;365 MB/s&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;hdparm /dev/sda1&lt;/STRONG&gt;&lt;BR /&gt;-sh: hdparm: command not found&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;BR /&gt;I saw an article called [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/USB-3-0-performance-on-iMX8M/m-p/838720" target="_self"&gt;USB 3.0 performance on iMX8M&lt;/A&gt;] on the NXP Community.&lt;BR /&gt;In this article, the theoretical speed of USB 3.0 is 500 MB/s, but in iMX8M it is described as 150-170 MB/s.&lt;BR /&gt;But the speeds I currently tested are 350-360 MB/s.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the maximum speed of USB 3.0 350-360 MB/s on the current i.MX 8M?&lt;BR /&gt;Can I get more speed of USB 3.0 on i.MX 8M with professional service?&lt;BR /&gt;BSP of i.MX 8M is using version 5.4.70_2.3.2.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Kwon&lt;/P&gt;</description>
    <pubDate>Tue, 26 Oct 2021 07:16:27 GMT</pubDate>
    <dc:creator>xoduddk123</dc:creator>
    <dc:date>2021-10-26T07:16:27Z</dc:date>
    <item>
      <title>USB 3.0 Performance on i.MX 8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-3-0-Performance-on-i-MX-8M/m-p/1361401#M182125</link>
      <description>&lt;P&gt;Hi, NXP Support Team.&lt;/P&gt;&lt;P&gt;I have an i.MX 8MQ development board.&lt;BR /&gt;I bought a USB 3.0 external hard case and NVMe M.2 SSD to test the USB 3.0 speed.&lt;BR /&gt;&lt;FONT size="2"&gt;USB 3.0 External Hard Case: RevuAhn UX980&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;NVMe M.2 SSD: Samsung 970 EVO Plus M.2 NVMe SSD 250GB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;The speed of the purchased external hard drive was checked from the USB 3.1(USB 3.2 Gen 2) port on the desktop.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVMe.png" style="width: 482px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160148i30476AD83878CE5F/image-size/large?v=v2&amp;amp;px=999" role="button" title="NVMe.png" alt="NVMe.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I did a speed test of the USB 3.0 external hard drive on the i.MX 8M development board with the dd command.&lt;BR /&gt;But the speed came out lower than I expected. Since it is USB 3.0, I expected a speed close to 500 MB/s.&lt;/P&gt;&lt;TABLE border="1" width="100%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="100%" height="1873px"&gt;root@imx8mqevk:~# &lt;STRONG&gt;uname -a&lt;/STRONG&gt;&lt;BR /&gt;Linux imx8mqevk 5.4.70 #49 SMP PREEMPT Tue Oct 26 15:28:23 KST 2021 aarch64 aarch64 aarch64 GNU/Linux&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;[ 80.213250] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd&lt;BR /&gt;[ 80.246101] scsi host0: uas&lt;BR /&gt;[ 80.249722] scsi 0:0:0:0: Direct-Access RevuAhn UX980 0208 PQ: 0 ANSI: 6&lt;BR /&gt;[ 82.232773] sd 0:0:0:0: [sda] 488397168 512-byte logical blocks: (250 GB/233 GiB)&lt;BR /&gt;[ 82.240303] sd 0:0:0:0: [sda] 4096-byte physical blocks&lt;BR /&gt;[ 82.246092] sd 0:0:0:0: [sda] Write Protect is off&lt;BR /&gt;[ 82.251552] sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA&lt;BR /&gt;[ 82.261282] sd 0:0:0:0: [sda] Optimal transfer size 33553920 bytes not a multiple of physical block size (4096 bytes)&lt;BR /&gt;[ 82.296370] sda: sda1&lt;BR /&gt;[ 82.300315] sd 0:0:0:0: [sda] Attached SCSI disk&lt;BR /&gt;[ 82.598946] EXT4-fs (sda1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;df -h&lt;/STRONG&gt;&lt;BR /&gt;Filesystem Size Used Avail Use% Mounted on&lt;BR /&gt;/dev/root 5.5G 3.4G 1.8G 66% /&lt;BR /&gt;devtmpfs 994M 4.0K 994M 1% /dev&lt;BR /&gt;tmpfs 1.5G 0 1.5G 0% /dev/shm&lt;BR /&gt;tmpfs 1.5G 9.0M 1.5G 1% /run&lt;BR /&gt;tmpfs 1.5G 0 1.5G 0% /sys/fs/cgroup&lt;BR /&gt;tmpfs 1.5G 4.0K 1.5G 1% /tmp&lt;BR /&gt;tmpfs 1.5G 188K 1.5G 1% /var/volatile&lt;BR /&gt;/dev/mmcblk0p1 84M 30M 54M 36% /run/media/mmcblk0p1&lt;BR /&gt;/dev/mmcblk0p2 5.5G 3.9G 1.4G 75% /run/media/mmcblk0p2&lt;BR /&gt;/dev/mmcblk1p1 84M 30M 54M 36% /run/media/mmcblk1p1&lt;BR /&gt;tmpfs 296M 8.0K 296M 1% /run/user/0&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;/dev/sda1 230G 4.1G 214G 2% /run/media/sda1&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;mount&lt;/STRONG&gt;&lt;BR /&gt;/dev/mmcblk1p2 on / type ext4 (rw,relatime)&lt;BR /&gt;devtmpfs on /dev type devtmpfs (rw,relatime,size=1017540k,nr_inodes=254385,mode=755)&lt;BR /&gt;sysfs on /sys type sysfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;proc on /proc type proc (rw,relatime)&lt;BR /&gt;securityfs on /sys/kernel/security type securityfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /dev/shm type tmpfs (rw,nosuid,nodev)&lt;BR /&gt;devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620,ptmxmode=000)&lt;BR /&gt;tmpfs on /run type tmpfs (rw,nosuid,nodev,mode=755)&lt;BR /&gt;tmpfs on /sys/fs/cgroup type tmpfs (ro,nosuid,nodev,noexec,mode=755)&lt;BR /&gt;cgroup2 on /sys/fs/cgroup/unified type cgroup2 (rw,nosuid,nodev,noexec,relatime,nsdelegate)&lt;BR /&gt;cgroup on /sys/fs/cgroup/systemd type cgroup (rw,nosuid,nodev,noexec,relatime,xattr,name=systemd)&lt;BR /&gt;pstore on /sys/fs/pstore type pstore (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;cgroup on /sys/fs/cgroup/hugetlb type cgroup (rw,nosuid,nodev,noexec,relatime,hugetlb)&lt;BR /&gt;cgroup on /sys/fs/cgroup/cpu,cpuacct type cgroup (rw,nosuid,nodev,noexec,relatime,cpu,cpuacct)&lt;BR /&gt;cgroup on /sys/fs/cgroup/pids type cgroup (rw,nosuid,nodev,noexec,relatime,pids)&lt;BR /&gt;cgroup on /sys/fs/cgroup/blkio type cgroup (rw,nosuid,nodev,noexec,relatime,blkio)&lt;BR /&gt;cgroup on /sys/fs/cgroup/cpuset type cgroup (rw,nosuid,nodev,noexec,relatime,cpuset)&lt;BR /&gt;cgroup on /sys/fs/cgroup/memory type cgroup (rw,nosuid,nodev,noexec,relatime,memory)&lt;BR /&gt;cgroup on /sys/fs/cgroup/devices type cgroup (rw,nosuid,nodev,noexec,relatime,devices)&lt;BR /&gt;cgroup on /sys/fs/cgroup/perf_event type cgroup (rw,nosuid,nodev,noexec,relatime,perf_event)&lt;BR /&gt;hugetlbfs on /dev/hugepages type hugetlbfs (rw,relatime,pagesize=2M)&lt;BR /&gt;mqueue on /dev/mqueue type mqueue (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;debugfs on /sys/kernel/debug type debugfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /tmp type tmpfs (rw,nosuid,nodev)&lt;BR /&gt;configfs on /sys/kernel/config type configfs (rw,nosuid,nodev,noexec,relatime)&lt;BR /&gt;tmpfs on /var/volatile type tmpfs (rw,relatime)&lt;BR /&gt;/dev/mmcblk0p1 on /run/media/mmcblk0p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;BR /&gt;/dev/mmcblk0p2 on /run/media/mmcblk0p2 type ext4 (rw,relatime)&lt;BR /&gt;/dev/mmcblk1p1 on /run/media/mmcblk1p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;BR /&gt;tmpfs on /run/user/0 type tmpfs (rw,nosuid,nodev,relatime,size=302092k,mode=700)&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;/dev/sda1 on /run/media/sda1 type ext4 (rw,relatime)&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;echo 3 &amp;gt; /proc/sys/vm/drop_caches&lt;/STRONG&gt;&lt;BR /&gt;[ 182.039954] sh (632): drop_caches: 3&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;sync ; dd if=/dev/zero of=/run/media/sda1/largefile bs=1G count=4 oflag=direct ; sync&lt;/STRONG&gt;&lt;BR /&gt;4+0 records in&lt;BR /&gt;4+0 records out&lt;BR /&gt;4294967296 bytes (4.3 GB, 4.0 GiB) copied, 12.2417 s, &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;351 MB/s&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~#&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;sync ; dd if=/run/media/sda1/largefile of=/dev/null bs=1G count=4 ; sync&lt;/STRONG&gt;&lt;BR /&gt;4+0 records in&lt;BR /&gt;4+0 records out&lt;BR /&gt;4294967296 bytes (4.3 GB, 4.0 GiB) copied, 11.7799 s, &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;365 MB/s&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;root@imx8mqevk:~# &lt;STRONG&gt;hdparm /dev/sda1&lt;/STRONG&gt;&lt;BR /&gt;-sh: hdparm: command not found&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;BR /&gt;I saw an article called [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/USB-3-0-performance-on-iMX8M/m-p/838720" target="_self"&gt;USB 3.0 performance on iMX8M&lt;/A&gt;] on the NXP Community.&lt;BR /&gt;In this article, the theoretical speed of USB 3.0 is 500 MB/s, but in iMX8M it is described as 150-170 MB/s.&lt;BR /&gt;But the speeds I currently tested are 350-360 MB/s.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the maximum speed of USB 3.0 350-360 MB/s on the current i.MX 8M?&lt;BR /&gt;Can I get more speed of USB 3.0 on i.MX 8M with professional service?&lt;BR /&gt;BSP of i.MX 8M is using version 5.4.70_2.3.2.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Kwon&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 07:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-3-0-Performance-on-i-MX-8M/m-p/1361401#M182125</guid>
      <dc:creator>xoduddk123</dc:creator>
      <dc:date>2021-10-26T07:16:27Z</dc:date>
    </item>
  </channel>
</rss>