<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックESAI receiver channels prioritization FIFO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ESAI-receiver-channels-prioritization-FIFO/m-p/1360871#M182071</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there a prioritization which receiver&amp;nbsp;channel is enqueuer in the SAI-Receive-FIFO first in case all 4-receiver channels are used in TDM Mode with external input clock?&lt;/P&gt;&lt;P&gt;Is it possible to read the FIFO via DMA without the ASRC Block?&lt;/P&gt;</description>
    <pubDate>Mon, 25 Oct 2021 12:51:58 GMT</pubDate>
    <dc:creator>M_MA</dc:creator>
    <dc:date>2021-10-25T12:51:58Z</dc:date>
    <item>
      <title>ESAI receiver channels prioritization FIFO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ESAI-receiver-channels-prioritization-FIFO/m-p/1360871#M182071</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there a prioritization which receiver&amp;nbsp;channel is enqueuer in the SAI-Receive-FIFO first in case all 4-receiver channels are used in TDM Mode with external input clock?&lt;/P&gt;&lt;P&gt;Is it possible to read the FIFO via DMA without the ASRC Block?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Oct 2021 12:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ESAI-receiver-channels-prioritization-FIFO/m-p/1360871#M182071</guid>
      <dc:creator>M_MA</dc:creator>
      <dc:date>2021-10-25T12:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: ESAI receiver channels prioritization FIFO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ESAI-receiver-channels-prioritization-FIFO/m-p/1362169#M182182</link>
      <description>&lt;P&gt;Hi Michael&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Is there a prioritization which receiver channel is enqueuer in the SAI-Receive-FIFO&lt;/P&gt;
&lt;P&gt;&amp;gt;first in case all 4-receiver channels are used in TDM Mode with external input clock?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there is no prioritization. From&amp;nbsp; sect.25.6.2 ESAI Receive Data Register (ESAI_ERDR) &lt;BR /&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX6DQRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"When multiple ESAI receivers are enabled, the data for each receiver is interleaved from lowest&lt;/P&gt;
&lt;P&gt;receiver to highest receiver (for example, if receivers 0, 2 and 3 are enabled then data is returned as follows: receiver #0, receiver #2, receiver #3, receiver #0, receiver #2, receiver #3, receiver #0, etc)."&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Is it possible to read the FIFO via DMA without the ASRC Block?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes, one can refer to sect.25.4.3 ESAI DMA Requests from the FIFOs.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 07:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ESAI-receiver-channels-prioritization-FIFO/m-p/1362169#M182182</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-27T07:02:31Z</dc:date>
    </item>
  </channel>
</rss>