<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does Imx6ull eLCDif support two different LCDs, using MPU mode and RGB mode? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-Imx6ull-eLCDif-support-two-different-LCDs-using-MPU-mode/m-p/1360322#M181990</link>
    <description>&lt;P&gt;Our current project usage scenario requires two LCD screens of different sizes. The interfaces of the two LCDs are different, one is an MPU 8080 interface, and the other is a 24-bit RGB interface. Can Imx6ull support the display of two display devices at the same time?&lt;/P&gt;</description>
    <pubDate>Sat, 23 Oct 2021 07:50:09 GMT</pubDate>
    <dc:creator>1405191257</dc:creator>
    <dc:date>2021-10-23T07:50:09Z</dc:date>
    <item>
      <title>Does Imx6ull eLCDif support two different LCDs, using MPU mode and RGB mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Imx6ull-eLCDif-support-two-different-LCDs-using-MPU-mode/m-p/1360322#M181990</link>
      <description>&lt;P&gt;Our current project usage scenario requires two LCD screens of different sizes. The interfaces of the two LCDs are different, one is an MPU 8080 interface, and the other is a 24-bit RGB interface. Can Imx6ull support the display of two display devices at the same time?&lt;/P&gt;</description>
      <pubDate>Sat, 23 Oct 2021 07:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Imx6ull-eLCDif-support-two-different-LCDs-using-MPU-mode/m-p/1360322#M181990</guid>
      <dc:creator>1405191257</dc:creator>
      <dc:date>2021-10-23T07:50:09Z</dc:date>
    </item>
  </channel>
</rss>