<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360131#M181975</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using 4.14.98 Sumo i.MX8M Mini board with qt 5.10.1,&amp;nbsp; X-Wayland Server.&lt;/P&gt;&lt;P&gt;When I'm trying to run qt application with combo-box, submenu. Application is terminating with&lt;/P&gt;&lt;P&gt;following errors when I click on it.&lt;/P&gt;&lt;P&gt;Using Wayland-EGL Using the 'xdg-shell-v6' shell integration zxdg_shell_v6@17: error 2: xdg_popup was not created on the topmost popup The Wayland connection experienced a fatal error (Protocol error).&lt;/P&gt;&lt;P&gt;How this error can be solved. Please do the needful.&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deeksha&lt;/P&gt;</description>
    <pubDate>Fri, 22 Oct 2021 13:54:16 GMT</pubDate>
    <dc:creator>deeksha</dc:creator>
    <dc:date>2021-10-22T13:54:16Z</dc:date>
    <item>
      <title>Wayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360131#M181975</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using 4.14.98 Sumo i.MX8M Mini board with qt 5.10.1,&amp;nbsp; X-Wayland Server.&lt;/P&gt;&lt;P&gt;When I'm trying to run qt application with combo-box, submenu. Application is terminating with&lt;/P&gt;&lt;P&gt;following errors when I click on it.&lt;/P&gt;&lt;P&gt;Using Wayland-EGL Using the 'xdg-shell-v6' shell integration zxdg_shell_v6@17: error 2: xdg_popup was not created on the topmost popup The Wayland connection experienced a fatal error (Protocol error).&lt;/P&gt;&lt;P&gt;How this error can be solved. Please do the needful.&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deeksha&lt;/P&gt;</description>
      <pubDate>Fri, 22 Oct 2021 13:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360131#M181975</guid>
      <dc:creator>deeksha</dc:creator>
      <dc:date>2021-10-22T13:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: Wayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360434#M182018</link>
      <description>&lt;P&gt;I tested xdg-shell-v6 on L5.10.XX and there is no issue when run qt demo.You can try newest BSP&lt;/P&gt;</description>
      <pubDate>Mon, 25 Oct 2021 02:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360434#M182018</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-10-25T02:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: Wayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360594#M182034</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;As I'm working L4.14.98 , cannot update BSP due to internal reason.&lt;/P&gt;&lt;P&gt;So could you please help me in resolve this issue.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deeksha&lt;/P&gt;</description>
      <pubDate>Mon, 25 Oct 2021 06:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-Protocol-error-Popups-created-with-parent-which-is-not/m-p/1360594#M182034</guid>
      <dc:creator>deeksha</dc:creator>
      <dc:date>2021-10-25T06:39:02Z</dc:date>
    </item>
  </channel>
</rss>