<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error Building U-boot v2020.04 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-U-boot-v2020-04/m-p/1359419#M181884</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Requirement:&lt;/STRONG&gt; Porting U-boot v2020.04 (released part of Kernel 5.4.70_2.3.0) from U-boot v2017.03 (released part of Kernel 4.1.15_2.0.0_ga).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Task performed:&lt;/STRONG&gt; Took the bb files of U-boot v2020.04 from EVK BSP (kernel 5.4.70_2.3.0) and tried building the U-boot.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Build failed:&lt;/STRONG&gt;&amp;nbsp;ERROR: Nothing PROVIDES 'python-native'.&amp;nbsp;Close matches:&lt;BR /&gt;python3-native&lt;BR /&gt;python3-py-native&lt;BR /&gt;python3-six-native&lt;BR /&gt;ERROR: Required build target 'u-boot' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['u-boot', 'python-native']&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Environment:&lt;/STRONG&gt; Ubuntu 18.04.1, Yocto project (not standalone)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Packages installed&lt;/STRONG&gt; (as recommended in Yocto Project User guide released as part Kernel 5.4.70) :&lt;/P&gt;&lt;P&gt;sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \&lt;BR /&gt;build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \&lt;BR /&gt;xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \&lt;BR /&gt;pylint3 xterm&lt;/P&gt;&lt;P&gt;Kindly help to solve the setup issue.&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;</description>
    <pubDate>Thu, 21 Oct 2021 10:03:01 GMT</pubDate>
    <dc:creator>arunkumar_maniv</dc:creator>
    <dc:date>2021-10-21T10:03:01Z</dc:date>
    <item>
      <title>Error Building U-boot v2020.04</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-U-boot-v2020-04/m-p/1359419#M181884</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Requirement:&lt;/STRONG&gt; Porting U-boot v2020.04 (released part of Kernel 5.4.70_2.3.0) from U-boot v2017.03 (released part of Kernel 4.1.15_2.0.0_ga).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Task performed:&lt;/STRONG&gt; Took the bb files of U-boot v2020.04 from EVK BSP (kernel 5.4.70_2.3.0) and tried building the U-boot.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Build failed:&lt;/STRONG&gt;&amp;nbsp;ERROR: Nothing PROVIDES 'python-native'.&amp;nbsp;Close matches:&lt;BR /&gt;python3-native&lt;BR /&gt;python3-py-native&lt;BR /&gt;python3-six-native&lt;BR /&gt;ERROR: Required build target 'u-boot' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['u-boot', 'python-native']&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Environment:&lt;/STRONG&gt; Ubuntu 18.04.1, Yocto project (not standalone)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Packages installed&lt;/STRONG&gt; (as recommended in Yocto Project User guide released as part Kernel 5.4.70) :&lt;/P&gt;&lt;P&gt;sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \&lt;BR /&gt;build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \&lt;BR /&gt;xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \&lt;BR /&gt;pylint3 xterm&lt;/P&gt;&lt;P&gt;Kindly help to solve the setup issue.&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;</description>
      <pubDate>Thu, 21 Oct 2021 10:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-U-boot-v2020-04/m-p/1359419#M181884</guid>
      <dc:creator>arunkumar_maniv</dc:creator>
      <dc:date>2021-10-21T10:03:01Z</dc:date>
    </item>
  </channel>
</rss>