<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック[IMX8mq custom board] pcie error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mq-custom-board-pcie-error/m-p/1356076#M181581</link>
    <description>&lt;P&gt;I am trying to insert wifi of qca9982 chip through pcie in IMX8MQ custom board.&lt;/P&gt;&lt;P&gt;However, pcie is not registered normally with the following message output:&lt;/P&gt;&lt;P&gt;[ 1.656089] imx6q-pcie 33800000.pcie: couldn't get pcie-phy&lt;/P&gt;&lt;P&gt;[ 1.693725] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:&lt;BR /&gt;[ 1.707218] imx6q-pcie 33800000.pcie: Parsing ranges property...&lt;BR /&gt;[ 1.707239] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 1.714673] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -&amp;gt; 0x18000000&lt;/P&gt;&lt;P&gt;[ 1.837606] imx6q-pcie 33800000.pcie: PCIe PLL locked after 0 us.&lt;/P&gt;&lt;P&gt;[ 2.974608] imx6q-pcie 33800000.pcie: Phy link never came up&lt;/P&gt;&lt;P&gt;[ 2.987892] imx6q-pcie 33800000.pcie: failed to initialize host&lt;BR /&gt;[ 2.993888] imx6q-pcie 33800000.pcie: unable to add pcie port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As a result of debugging pci-imx6.c, the result value is returned as -ENODEV(-19) in the process of calling the dw_pcie_host_init() function. Please check if there are any additional things to check.&lt;/P&gt;</description>
    <pubDate>Fri, 15 Oct 2021 00:33:36 GMT</pubDate>
    <dc:creator>jhii6488_vine</dc:creator>
    <dc:date>2021-10-15T00:33:36Z</dc:date>
    <item>
      <title>[IMX8mq custom board] pcie error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mq-custom-board-pcie-error/m-p/1356076#M181581</link>
      <description>&lt;P&gt;I am trying to insert wifi of qca9982 chip through pcie in IMX8MQ custom board.&lt;/P&gt;&lt;P&gt;However, pcie is not registered normally with the following message output:&lt;/P&gt;&lt;P&gt;[ 1.656089] imx6q-pcie 33800000.pcie: couldn't get pcie-phy&lt;/P&gt;&lt;P&gt;[ 1.693725] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:&lt;BR /&gt;[ 1.707218] imx6q-pcie 33800000.pcie: Parsing ranges property...&lt;BR /&gt;[ 1.707239] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 1.714673] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -&amp;gt; 0x18000000&lt;/P&gt;&lt;P&gt;[ 1.837606] imx6q-pcie 33800000.pcie: PCIe PLL locked after 0 us.&lt;/P&gt;&lt;P&gt;[ 2.974608] imx6q-pcie 33800000.pcie: Phy link never came up&lt;/P&gt;&lt;P&gt;[ 2.987892] imx6q-pcie 33800000.pcie: failed to initialize host&lt;BR /&gt;[ 2.993888] imx6q-pcie 33800000.pcie: unable to add pcie port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As a result of debugging pci-imx6.c, the result value is returned as -ENODEV(-19) in the process of calling the dw_pcie_host_init() function. Please check if there are any additional things to check.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 00:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mq-custom-board-pcie-error/m-p/1356076#M181581</guid>
      <dc:creator>jhii6488_vine</dc:creator>
      <dc:date>2021-10-15T00:33:36Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8mq custom board] pcie error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8mq-custom-board-pcie-error/m-p/1356198#M181590</link>
      <description>&lt;P&gt;Hi Hyein&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to narrow down issue, if this is caused by pcie card or custom board.&lt;/P&gt;
&lt;P&gt;For example try with several pcie card. For board please recheck pcie recommendations&lt;/P&gt;
&lt;P&gt;provided in&amp;nbsp; &lt;A id="relatedDocsClick_6" href="https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8MDQLQ Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 05:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8mq-custom-board-pcie-error/m-p/1356198#M181590</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-15T05:48:28Z</dc:date>
    </item>
  </channel>
</rss>