<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Serial Download - Internal Boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-Internal-Boot/m-p/1356018#M181573</link>
    <description>&lt;P&gt;Hi, I'm working with an IMXRT1050 and I need to make an image writing by the MCUXpresso Secure Provisioning software. To do this, I set the kit startup to serial download. After burning, the image will only run if I manually change boot to internal boot. I would like to know if it is possible to keep the boot in Serial Download, write the image and run the image without manually switching to internal boot&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 18:52:22 GMT</pubDate>
    <dc:creator>pauloisaia</dc:creator>
    <dc:date>2021-10-14T18:52:22Z</dc:date>
    <item>
      <title>Serial Download - Internal Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-Internal-Boot/m-p/1356018#M181573</link>
      <description>&lt;P&gt;Hi, I'm working with an IMXRT1050 and I need to make an image writing by the MCUXpresso Secure Provisioning software. To do this, I set the kit startup to serial download. After burning, the image will only run if I manually change boot to internal boot. I would like to know if it is possible to keep the boot in Serial Download, write the image and run the image without manually switching to internal boot&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 18:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-Internal-Boot/m-p/1356018#M181573</guid>
      <dc:creator>pauloisaia</dc:creator>
      <dc:date>2021-10-14T18:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Download - Internal Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-Internal-Boot/m-p/1359025#M181844</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;It is necessary to switch to internal boot to run the image. &lt;BR /&gt;There is some exception when you are using MCUXpresoo with a board. You can open a debug session while you are in serial download and the application runs while the debug session is open.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 22:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Download-Internal-Boot/m-p/1359025#M181844</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-10-20T22:48:54Z</dc:date>
    </item>
  </channel>
</rss>