<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where is core-image recipe ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/1355908#M181567</link>
    <description>&lt;P&gt;The "core-image" class is defined in poky/meta/classes/core-image.bbclass, this is the class that core-image-minimal.bb recipe inherits from.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 14:29:16 GMT</pubDate>
    <dc:creator>eol</dc:creator>
    <dc:date>2021-10-14T14:29:16Z</dc:date>
    <item>
      <title>Where is core-image recipe ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570412#M87552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where is core-image recipe? If i see core-image-minimal.bb,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SUMMARY = "A small image just capable of allowing a device to boot."&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL = "packagegroup-core-boot ${ROOTFS_PKGMANAGE_BOOTSTRAP} ${CORE_IMAGE_EXTRA_INSTALL}"&lt;/P&gt;&lt;P&gt;IMAGE_LINGUAS = " "&lt;/P&gt;&lt;P&gt;LICENSE = "MIT"&lt;/P&gt;&lt;P&gt;inherit core-image&lt;/P&gt;&lt;P&gt;IMAGE_ROOTFS_SIZE ?= "8192"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So where is it getting all the packages from? If i have to see and edit the packages it is downloading where should i look at??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 10:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570412#M87552</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2016-06-24T10:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Where is core-image recipe ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570413#M87553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manjunath,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following links may be helpful:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331917"&gt;How to add a new layer and a new recipe in Yocto&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1616"&gt;Freescale Yocto Project main page&lt;/A&gt; &lt;/P&gt;&lt;P&gt; &lt;A href="https://community.nxp.com/thread/394705"&gt;Can we add Debian packages(Package_deb) in Yocto build?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 15:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570413#M87553</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-06-28T15:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: Where is core-image recipe ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570414#M87554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply. I really appreciate the third link you have sent me. But my question was where is the core-image actually?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Means, let me put it this way,&lt;/P&gt;&lt;P&gt;core-image-sato&lt;/P&gt;&lt;P&gt;core-image-x11&lt;/P&gt;&lt;P&gt;core-image-base&lt;/P&gt;&lt;P&gt;core-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the above recipes use "core-image" as inherited common image. I hope you agree. Now, where is that ? I tried to grep but couldn't find.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 11:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570414#M87554</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2016-06-29T11:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: Where is core-image recipe ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570415#M87555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe&amp;nbsp; "inherit" means that they inherit the class "core-image" and not a recipe by that name,&amp;nbsp; This class is likely located somewhere in the yocto python source code. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2017 13:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/570415#M87555</guid>
      <dc:creator>5frank</dc:creator>
      <dc:date>2017-10-20T13:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: Where is core-image recipe ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/1355908#M181567</link>
      <description>&lt;P&gt;The "core-image" class is defined in poky/meta/classes/core-image.bbclass, this is the class that core-image-minimal.bb recipe inherits from.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 14:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-is-core-image-recipe/m-p/1355908#M181567</guid>
      <dc:creator>eol</dc:creator>
      <dc:date>2021-10-14T14:29:16Z</dc:date>
    </item>
  </channel>
</rss>