<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: insmod ds1339.ko failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/insmod-ds1339-ko-failed/m-p/1355690#M181542</link>
    <description>&lt;P&gt;add:&lt;/P&gt;&lt;P&gt;the firmware downloaded to the two boards are the same one,hasn't any difference.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 08:30:17 GMT</pubDate>
    <dc:creator>18890366157</dc:creator>
    <dc:date>2021-10-14T08:30:17Z</dc:date>
    <item>
      <title>insmod ds1339.ko failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/insmod-ds1339-ko-failed/m-p/1355689#M181541</link>
      <description>&lt;P&gt;my platform is IMX6ULL.&lt;/P&gt;&lt;P&gt;I wrote an i2c device driver program called ds1339.c 3 days earlier,and I could find ds1339 under /dev after insmod ds1339.ko,but I couldn't find ds1339 now,it's very strange.&lt;/P&gt;&lt;P&gt;I tried to program the whole system firmware to my development board which has the same core,and I could find ds1339 under /dev after insmod ds1339.ko.&lt;/P&gt;&lt;P&gt;so,what's the cause of this weird thing??&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 08:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/insmod-ds1339-ko-failed/m-p/1355689#M181541</guid>
      <dc:creator>18890366157</dc:creator>
      <dc:date>2021-10-14T08:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: insmod ds1339.ko failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/insmod-ds1339-ko-failed/m-p/1355690#M181542</link>
      <description>&lt;P&gt;add:&lt;/P&gt;&lt;P&gt;the firmware downloaded to the two boards are the same one,hasn't any difference.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 08:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/insmod-ds1339-ko-failed/m-p/1355690#M181542</guid>
      <dc:creator>18890366157</dc:creator>
      <dc:date>2021-10-14T08:30:17Z</dc:date>
    </item>
  </channel>
</rss>