<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTwo camera input on i.MX RT1170</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1355639#M181536</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to show 2 camera view on panel same time. The concept as below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 338px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159088i946B254DD62569CC/image-dimensions/338x197?v=v2" width="338" height="197" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And I found the this picture as below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 331px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159089i60F671EDB4BBB74E/image-dimensions/331x334?v=v2" width="331" height="334" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So...maybe i.MX RT1170 can't support 2 camera input as same time? Or it is possible but MCU must high speed switch VIDEO_MUX?&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 07:30:04 GMT</pubDate>
    <dc:creator>scarletlee</dc:creator>
    <dc:date>2021-10-14T07:30:04Z</dc:date>
    <item>
      <title>Two camera input on i.MX RT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1355639#M181536</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to show 2 camera view on panel same time. The concept as below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 338px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159088i946B254DD62569CC/image-dimensions/338x197?v=v2" width="338" height="197" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And I found the this picture as below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 331px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159089i60F671EDB4BBB74E/image-dimensions/331x334?v=v2" width="331" height="334" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So...maybe i.MX RT1170 can't support 2 camera input as same time? Or it is possible but MCU must high speed switch VIDEO_MUX?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 07:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1355639#M181536</guid>
      <dc:creator>scarletlee</dc:creator>
      <dc:date>2021-10-14T07:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: Two camera input on i.MX RT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1356235#M181597</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/177381"&gt;@scarletlee&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Your understanding is correct!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;When you use two camera, even one connect to MIPI-CSI, another connect to the parallel CSI module, you still can't work it at the same time. As you see,&amp;nbsp;&amp;nbsp;MIPI-CSI and parrallel CSI at last connect to the CSI module, so you can't make the two camea input at the same time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;So, another solution is use the flexIO connect the second camera.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You can refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12686.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12686.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;If you still have questions about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 06:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-camera-input-on-i-MX-RT1170/m-p/1356235#M181597</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-10-15T06:51:08Z</dc:date>
    </item>
  </channel>
</rss>