<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8X SCFW RTC IRQ handler in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1355120#M181496</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using i.MX 8X and SCFW version 1.7.1. I would like to know whether the internal RTC's interrupts are enabled by default or if they need to be explicitly enabled via sc_irq_enable. Also, is there a dedicated IRQ handler for those interrupts or do we have to periodically check them via sc_irq_status?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petar&lt;/P&gt;</description>
    <pubDate>Wed, 13 Oct 2021 15:59:44 GMT</pubDate>
    <dc:creator>petar_petrov</dc:creator>
    <dc:date>2021-10-13T15:59:44Z</dc:date>
    <item>
      <title>i.MX 8X SCFW RTC IRQ handler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1355120#M181496</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using i.MX 8X and SCFW version 1.7.1. I would like to know whether the internal RTC's interrupts are enabled by default or if they need to be explicitly enabled via sc_irq_enable. Also, is there a dedicated IRQ handler for those interrupts or do we have to periodically check them via sc_irq_status?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Petar&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 15:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1355120#M181496</guid>
      <dc:creator>petar_petrov</dc:creator>
      <dc:date>2021-10-13T15:59:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8X SCFW RTC IRQ handler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1357753#M181759</link>
      <description>&lt;P&gt;Hi Petar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt; whether the internal RTC's interrupts are enabled by defaul..&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;no&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;or if they need to be explicitly enabled via sc_irq_enable.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt; is there a dedicated IRQ handler for those interrupt..&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;no&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;or do we have to periodically check them via sc_irq_status?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 08:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1357753#M181759</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-19T08:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8X SCFW RTC IRQ handler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1357895#M181771</link>
      <description>&lt;P&gt;Hello, Igor,&lt;/P&gt;&lt;P&gt;Thank you for the reply! I was also wondering which resource needs to be passed when enabling the RTC interrupts and checking their status?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Petar&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 12:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8X-SCFW-RTC-IRQ-handler/m-p/1357895#M181771</guid>
      <dc:creator>petar_petrov</dc:creator>
      <dc:date>2021-10-19T12:21:10Z</dc:date>
    </item>
  </channel>
</rss>