<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEnabling Cache for display module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Cache-for-display-module/m-p/1353409#M181344</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to know how disabling the cache (SCB_DisableDCache()) will affect the performance of the LCD display. If I disable the cache the update gets slower. On enabling cache the display update is faster but the pixels are not updated properly on the first refresh when a screen is changed. Also the USB host functionality does not enumerate the mouse if cache is enabled. How to solve this issue?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 11 Oct 2021 09:02:47 GMT</pubDate>
    <dc:creator>EmbeddedTech</dc:creator>
    <dc:date>2021-10-11T09:02:47Z</dc:date>
    <item>
      <title>Enabling Cache for display module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Cache-for-display-module/m-p/1353409#M181344</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to know how disabling the cache (SCB_DisableDCache()) will affect the performance of the LCD display. If I disable the cache the update gets slower. On enabling cache the display update is faster but the pixels are not updated properly on the first refresh when a screen is changed. Also the USB host functionality does not enumerate the mouse if cache is enabled. How to solve this issue?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Oct 2021 09:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Cache-for-display-module/m-p/1353409#M181344</guid>
      <dc:creator>EmbeddedTech</dc:creator>
      <dc:date>2021-10-11T09:02:47Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling Cache for display module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Cache-for-display-module/m-p/1361140#M182097</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you to refer to the &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12042.pdf" target="_self"&gt;application note&lt;/A&gt; to learn the cache feature, further, the application note also guides users on how to use cache to develop applications running in a correct and high-performance way.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 02:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Cache-for-display-module/m-p/1361140#M182097</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-10-26T02:00:25Z</dc:date>
    </item>
  </channel>
</rss>