<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 and fullHD resolution (1920x1080), wrong application window in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233666#M18123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;was your image (uboot + kernel + rootfs) built with Yocto framework?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jun 2013 14:57:39 GMT</pubDate>
    <dc:creator>LeonardoSandova</dc:creator>
    <dc:date>2013-06-21T14:57:39Z</dc:date>
    <item>
      <title>iMX6 and fullHD resolution (1920x1080), wrong application window</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233665#M18122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I was trying to run 1920x1080 on my Wandboard (iMX6DL) I found out that in fact the resolution came up. &lt;/P&gt;&lt;P&gt;But the wallpaper window and all application windows were not as high as they could be, i.e. approximately 720 lines instead of 1080-48 lines (bottom, system bar is as far as I know 48 pixel at 160dpi). &lt;/P&gt;&lt;P&gt;I suspect it is the layout of the launcher. Unfortunately I have only a few experience with xml layout files.&lt;/P&gt;&lt;P&gt;- Did anybody face the same issues?&lt;/P&gt;&lt;P&gt;- Has someone found a solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 14:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233665#M18122</guid>
      <dc:creator>blauer</dc:creator>
      <dc:date>2013-06-21T14:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 and fullHD resolution (1920x1080), wrong application window</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233666#M18123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;was your image (uboot + kernel + rootfs) built with Yocto framework?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 14:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233666#M18123</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-06-21T14:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 and fullHD resolution (1920x1080), wrong application window</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233667#M18124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Leonardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be honest: no clue.&lt;/P&gt;&lt;P&gt;I am using the Wandboard sources 4.1.2 and the April patch.&lt;/P&gt;&lt;P&gt;Did not change anything except the /device/fslwandboard/Bootconfig.mk file. Just changed the BOARD_KERNEL_CMDLINE to&lt;/P&gt;&lt;P&gt;&lt;EM&gt;BOARD_KERNEL_CMDLINE := console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=28M vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then set "lunch 17" (Wandboard user)&lt;/P&gt;&lt;P&gt;and started to "make"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 15:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-and-fullHD-resolution-1920x1080-wrong-application-window/m-p/233667#M18124</guid>
      <dc:creator>blauer</dc:creator>
      <dc:date>2013-06-21T15:13:35Z</dc:date>
    </item>
  </channel>
</rss>