<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Design Files for i.MX8 plus Base Board: Netlist update</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350610#M181064</link>
    <description>&lt;P&gt;Netlist update to Layout shows nine warnings, all of this type: WARNING(SPMHNI-295): Component 'R108', property 'SIGNAL_MODEL'. Value 'DEFAULT_RESISTOR_100000OHM_2_1' was overwritten by 'DEFAULT_RESISTOR_33.000000OHM_2_1'.&lt;/P&gt;&lt;P&gt;See attachment. I'd want to know whether I should do anything with it, or if it can be ignored. It should however be noted that the Layout file is updated by OrCAD from 17.2 to version 17.4 format.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Oct 2021 12:46:01 GMT</pubDate>
    <dc:creator>rjm</dc:creator>
    <dc:date>2021-10-05T12:46:01Z</dc:date>
    <item>
      <title>Design Files for i.MX8 plus Base Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350606#M181062</link>
      <description>&lt;P&gt;Download location: &lt;A href="https://www.nxp.com/webapp/Download?colCode=8MPLUS-BB" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=8MPLUS-BB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;(accompanying CPU-board: &lt;A href="https://www.nxp.com/webapp/Download?colCode=8MPLUSLPD4-CPU" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=8MPLUSLPD4-CPU&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;Portal entry: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Portal-entry-for-OrCAD-Design-Files-issues/m-p/1350579" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/Portal-entry-for-OrCAD-Design-Files-issues/m-p/1350579&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 12:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350606#M181062</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-10-27T12:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Design Files for i.MX8 plus Base Board: Netlist update</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350610#M181064</link>
      <description>&lt;P&gt;Netlist update to Layout shows nine warnings, all of this type: WARNING(SPMHNI-295): Component 'R108', property 'SIGNAL_MODEL'. Value 'DEFAULT_RESISTOR_100000OHM_2_1' was overwritten by 'DEFAULT_RESISTOR_33.000000OHM_2_1'.&lt;/P&gt;&lt;P&gt;See attachment. I'd want to know whether I should do anything with it, or if it can be ignored. It should however be noted that the Layout file is updated by OrCAD from 17.2 to version 17.4 format.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 12:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350610#M181064</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-10-05T12:46:01Z</dc:date>
    </item>
    <item>
      <title>Re: Design Files for i.MX8 plus Base Board: Netlist update</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350874#M181099</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181692"&gt;@rjm&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; Generally the warnings may be omitted. Nevertheless, please check&lt;BR /&gt;(PCB) size of overwritten elements - it should not occupy more space on board.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 03:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1350874#M181099</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-10-06T03:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: Design Files for i.MX8 plus Base Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1362437#M182209</link>
      <description>&lt;P&gt;When I want to re-route parts of the board, especially differential pairs, the following is reported in the command window: &lt;U&gt;&lt;EM&gt;Timing feedback is disabled because timed based rules are not allowed. With this product, you must define delay rules in length units.&lt;/EM&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;I use &lt;STRONG&gt;OrCAD PCB Designer Professional &lt;/STRONG&gt;(17.4). The only product that goes beyond &lt;EM&gt;Professional&lt;/EM&gt; is Allegro instead of OrCAD. Any hints regarding the PCB Designer license variant used with NXP would be appriciated.&lt;/P&gt;&lt;P&gt;The above message also occurs on the CPU module board.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 12:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1362437#M182209</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-10-27T12:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: Design Files for i.MX8 plus Base Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1370559#M182975</link>
      <description>&lt;P&gt;Acccording to Flowcad, this shows that NXP is using the (highest end) Allegro PCB designer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Note: This answer is marked as "solution", but that does not apply to the posting as a whole - that's due to the attempt to establish a sort of umbrella posting that may handle several subtopics, as this one...&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Nov 2021 09:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Design-Files-for-i-MX8-plus-Base-Board/m-p/1370559#M182975</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-11-12T09:22:37Z</dc:date>
    </item>
  </channel>
</rss>