<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NXP ROM in open mode, Can not program Teensey 4.1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-ROM-in-open-mode-Can-not-program-Teensey-4-1/m-p/1350417#M181047</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/112157"&gt;@c172jeff&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I haven't Teensey4.1. I'm not sure what's the problem. RT1062 ROM code hasn't open mode.&lt;/P&gt;
&lt;P&gt;In&amp;nbsp;&lt;A href="https://www.pjrc.com/store/teensy41.html," target="_blank"&gt;https://www.pjrc.com/store/teensy41.html,&lt;/A&gt;&amp;nbsp;I see that this board has a dedicated bootloader chip. And there is a Program pushbutton.&amp;nbsp;&lt;SPAN&gt;Pressing the button button puts Teensy into programming mode. Can this work on your board? And Teensy 4.1 will fully erase its non-volatile memory and return the flash memory to a simple LED blink program if the program button is held between 13 to 17 seconds.&lt;/SPAN&gt;&amp;nbsp;If you can fully erase flash and power on again, Teensy Loader should can program the board.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Tue, 05 Oct 2021 07:33:59 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-10-05T07:33:59Z</dc:date>
    <item>
      <title>NXP ROM in open mode, Can not program Teensey 4.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-ROM-in-open-mode-Can-not-program-Teensey-4-1/m-p/1346321#M180635</link>
      <description>&lt;P&gt;Help.&amp;nbsp; This might not be the most ideal place to post this question.&amp;nbsp; I am stuck and need direction.&lt;/P&gt;&lt;P&gt;I bought a Teensey 4.1 board and programmed it a few times.&amp;nbsp; This board is similar to an Arduino but based on a fast chip with tons of features.&amp;nbsp; I guess it is an NXP chip.&lt;/P&gt;&lt;P&gt;I set it aside for a few months and am now looking to reprogram it.&amp;nbsp; I cannot.&amp;nbsp; It seems there is communication to the board but the board throws an error to the loader about NXP Memory&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;"23:31:18.259 (loader): Opps, NXP ROM in open mode, but we do not yet have code for this case&amp;nbsp;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I tried two known working USB cables am quite sure that there is communication.&amp;nbsp; I don't think it is a Windows 10 thing.&amp;nbsp; I am running Windows 10.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone on this forum provide some advice and offer suggestions?&amp;nbsp; I hate to buy a new $40 board when it seems flimsey enough that the ROM gets stuck in open mode.&amp;nbsp; What is ROM?&amp;nbsp; I know it is read only memory, but is this the flash memory that the loader is trying to program?&lt;/P&gt;&lt;P&gt;If so, is there a way that I can close it with an external circuit/connection and/or better code/tools?&lt;/P&gt;&lt;P&gt;I would like to use this Teensey, just that I have a problem throwing money at something that seems likely to repeat.&amp;nbsp; I treated this board nice.&lt;/P&gt;&lt;P&gt;Here is the log from the Teensey loader .&amp;nbsp; The loader asked to press a button, then it displayed the second section with the line of output above.&amp;nbsp; The button press on the Teensey triggered action on the loader.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.709 (loader): file changed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.727 (loader): File "C:\Users\Jeffrey\AppData\Local\Temp\arduino_build _195947\Example2_OutputToProcessing.ino.hex", 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.730 (loader): File "Example2_OutputToProcessing.ino.hex". 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.733 (post_compile 3): Begin, version=1.55, high-res time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.740 (loader): remote connection 11120 opened&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.742 (loader): remote cmd from 11120: "comment: Teensyduino 1.55 - WINDOWS (teensy_post_compile)"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.742 (post_compile 3): Sending command: comment: Teensyduino 1.55 - WINDOWS (teensy_post_compile)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.743 (loader): remote cmd from 11120: "status"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.751 (post_compile 3): Status: 1, 0, 0, 14, 0, 0, C:\Users\Jeffrey\AppData\Local\Temp\arduino_build_ 195947\, Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.751 (post_compile 3): Sending command: dir:C:\Users\Jeffrey\AppData\Local\Temp\arduino_bu ild_195947\&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.752 (loader): remote cmd from 11120: "dir:C:\Users\Jeffrey\AppData\Local\Temp\arduino_b uild_195947\"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.754 (loader): remote cmd from 11120: "file:Example2_OutputToProcessing.ino.hex"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.755 (post_compile 3): Sending command: file:Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.768 (loader): File "C:\Users\Jeffrey\AppData\Local\Temp\arduino_build _195947\Example2_OutputToProcessing.ino.hex", 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.770 (loader): File "Example2_OutputToProcessing.ino.hex". 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.774 (loader): remote cmd from 11120: "status"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.782 (post_compile 3): Status: 1, 0, 0, 14, 0, 0, C:\Users\Jeffrey\AppData\Local\Temp\arduino_build_ 195947\, Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.782 (post_compile 3): Sending command: auto&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;n&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.782 (loader): remote cmd from 11120: "auto&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;n"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.784 (post_compile 3): Disconnect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:50.807 (loader): remote connection 11120 closed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.138 (post_compile 4): Begin, version=1.55, high-res time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.140 (loader): remote connection 11124 opened&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.143 (loader): remote cmd from 11124: "comment: Teensyduino 1.55 - WINDOWS (teensy_post_compile)"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.144 (post_compile 4): Sending command: comment: Teensyduino 1.55 - WINDOWS (teensy_post_compile)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.146 (loader): remote cmd from 11124: "status"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.155 (loader): remote cmd from 11124: "dir:C:\Users\Jeffrey\AppData\Local\Temp\arduino_b uild_195947\"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.156 (post_compile 4): Status: 1, 1, 0, 14, 0, 0, C:\Users\Jeffrey\AppData\Local\Temp\arduino_build_ 195947\, Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.156 (post_compile 4): Sending command: dir:C:\Users\Jeffrey\AppData\Local\Temp\arduino_bu ild_195947\&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.158 (loader): remote cmd from 11124: "file:Example2_OutputToProcessing.ino.hex"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.159 (post_compile 4): Sending command: file:Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.172 (loader): File "C:\Users\Jeffrey\AppData\Local\Temp\arduino_build _195947\Example2_OutputToProcessing.ino.hex", 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.176 (loader): File "Example2_OutputToProcessing.ino.hex". 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.183 (loader): remote cmd from 11124: "status"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.193 (post_compile 4): Status: 1, 1, 0, 14, 0, 0, C:\Users\Jeffrey\AppData\Local\Temp\arduino_build_ 195947\, Example2_OutputToProcessing.ino.hex&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.193 (post_compile 4): Disconnect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.210 (post_compile 5): Running teensy_reboot: "C:\Program Files (x86)\Arduino\hardware\teensy\..\tools\teensy_rebo ot.exe" teensy_reboot.exe "-board=TEENSY41" "-port=fake serial" "-portlabel=(null)" "-portprotocol=(null)"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.215 (loader): remote connection 11124 closed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.225 (loader): remote connection 11124 opened&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): Begin, version=1.55, high-res time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): location = fake serial&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): portprotocol = (null)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): portlabel = (null)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): Emulated serial devices will be tried first&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): LoadLibrary cfgmgr32 ok&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.252 (reboot 6): LoadLibrary ntdll ok&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.254 (reboot 6): nothing new, skipping HID &amp;amp; Ports enum&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.258 (loader): remote connection 11128 opened&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.264 (reboot 6): Disconnect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.289 (loader): remote connection 11128 closed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:29:51.296 (loader): remote connection 11124 closed&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;After Button Press&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:17.864 (ports 2): WM_DEVICECHANGE DBT_DEVICEREMOVECOMPLETE&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:17.869 (ports 2): nothing new, skipping HID &amp;amp; Ports enum&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:17.882 (ports 2): WM_DEVICECHANGE DBT_DEVNODES_CHANGED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:17.883 (ports 2): nothing new, skipping HID &amp;amp; Ports enum&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:17.960 (loader): stop ignoring usb:0/1D0000/0/1/5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.045 (ports 2): WM_DEVICECHANGE DBT_DEVICEARRIVAL&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.045 (ports 2): nothing new, skipping HID &amp;amp; Ports enum&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.212 (loader): handle 2b40&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.214 (loader): Device came online, code_size = 100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.215 (loader): Board is: NXP IMXRT1062 ROM&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.218 (loader): begin operation&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.233 (loader): File "C:\Users\Jeffrey\AppData\Local\Temp\arduino_build _195947\Example2_OutputToProcessing.ino.hex", 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.236 (loader): File "Example2_OutputToProcessing.ino.hex". 33792 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.239 (loader): set background IMG_ONLINE&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.250 (loader): nxp_write: success&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.254 (loader): nxp_write: success&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.257 (loader): HAB open mode, bootcfg=80018&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.259 (loader): Opps, NXP ROM in open mode, but we do not yet have code for this case&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.261 (loader): start ignoring usb:0/1D0000/0/1/5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.264 (loader): end operation, total time = 0.043 seconds&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.270 (loader): redraw timer set, image 79 to show for 3000 ms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.287 (ports 2): WM_DEVICECHANGE DBT_DEVNODES_CHANGED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:18.287 (ports 2): nothing new, skipping HID &amp;amp; Ports enum&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;23:31:21.270 (loader): redraw, image 9&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
      <pubDate>Sun, 26 Sep 2021 13:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-ROM-in-open-mode-Can-not-program-Teensey-4-1/m-p/1346321#M180635</guid>
      <dc:creator>c172jeff</dc:creator>
      <dc:date>2021-09-26T13:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: NXP ROM in open mode, Can not program Teensey 4.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-ROM-in-open-mode-Can-not-program-Teensey-4-1/m-p/1350417#M181047</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/112157"&gt;@c172jeff&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I haven't Teensey4.1. I'm not sure what's the problem. RT1062 ROM code hasn't open mode.&lt;/P&gt;
&lt;P&gt;In&amp;nbsp;&lt;A href="https://www.pjrc.com/store/teensy41.html," target="_blank"&gt;https://www.pjrc.com/store/teensy41.html,&lt;/A&gt;&amp;nbsp;I see that this board has a dedicated bootloader chip. And there is a Program pushbutton.&amp;nbsp;&lt;SPAN&gt;Pressing the button button puts Teensy into programming mode. Can this work on your board? And Teensy 4.1 will fully erase its non-volatile memory and return the flash memory to a simple LED blink program if the program button is held between 13 to 17 seconds.&lt;/SPAN&gt;&amp;nbsp;If you can fully erase flash and power on again, Teensy Loader should can program the board.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 07:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-ROM-in-open-mode-Can-not-program-Teensey-4-1/m-p/1350417#M181047</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-10-05T07:33:59Z</dc:date>
    </item>
  </channel>
</rss>