<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB Communication between to self powered boards in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350129#M181016</link>
    <description>&lt;P&gt;Hi Everyone,&lt;BR /&gt;I'm working on a design and I'm not sure it will work properly.&lt;BR /&gt;Mainly because the USB is OTG and there is no VBUS connection between the boards.&lt;BR /&gt;I want to make a connection between two boards, each board has it's own power supply, there is no VBUS connection between the boards. One board will function as a master and the other as a device.&lt;BR /&gt;Does anyone have suggestions for repair/addition or advice on how to do it better?&lt;BR /&gt;I added a picture to illustrate the connection between the boards.&lt;/P&gt;</description>
    <pubDate>Mon, 04 Oct 2021 14:45:47 GMT</pubDate>
    <dc:creator>DSEngineer</dc:creator>
    <dc:date>2021-10-04T14:45:47Z</dc:date>
    <item>
      <title>USB Communication between to self powered boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350129#M181016</link>
      <description>&lt;P&gt;Hi Everyone,&lt;BR /&gt;I'm working on a design and I'm not sure it will work properly.&lt;BR /&gt;Mainly because the USB is OTG and there is no VBUS connection between the boards.&lt;BR /&gt;I want to make a connection between two boards, each board has it's own power supply, there is no VBUS connection between the boards. One board will function as a master and the other as a device.&lt;BR /&gt;Does anyone have suggestions for repair/addition or advice on how to do it better?&lt;BR /&gt;I added a picture to illustrate the connection between the boards.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Oct 2021 14:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350129#M181016</guid>
      <dc:creator>DSEngineer</dc:creator>
      <dc:date>2021-10-04T14:45:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication between to self powered boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350299#M181028</link>
      <description>&lt;P&gt;Hi Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for communication between two boards one can try to use usb unit tests, configure&lt;/P&gt;
&lt;P&gt;one board as host other as device:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=lf-5.10.52_2.1.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=lf-5.10.52_2.1.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 04 Oct 2021 23:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350299#M181028</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-04T23:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication between to self powered boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350396#M181041</link>
      <description>&lt;P&gt;Hi Igor,&lt;BR /&gt;Thanks for the help.&lt;BR /&gt;Yes,&amp;nbsp;I was thinking about this configuration, but when one is set as a device he does not expect to get 5V in VBUS? Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 06:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350396#M181041</guid>
      <dc:creator>DSEngineer</dc:creator>
      <dc:date>2021-10-05T06:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication between to self powered boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350447#M181049</link>
      <description>&lt;P&gt;&amp;gt;Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;on device side VBUS can be connected directly to 5V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 08:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Communication-between-to-self-powered-boards/m-p/1350447#M181049</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-05T08:16:36Z</dc:date>
    </item>
  </channel>
</rss>