<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX 8M Nano - AB Boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-Nano-AB-Boot/m-p/1349535#M180945</link>
    <description>&lt;P&gt;Hello support team,&lt;/P&gt;&lt;P&gt;we will work with a board based on the iMX 8M Nano processor and we are supposed to have a full AB Boot implemented. This would mean the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;two partitions which contain &lt;EM&gt;flash.bin&lt;/EM&gt; images&lt;/LI&gt;&lt;LI&gt;two &lt;EM&gt;boot&lt;/EM&gt; and &lt;EM&gt;root&lt;/EM&gt; partitions (though this isn't hard to do).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Question&lt;/STRONG&gt;: is there a way to tell the &lt;EM&gt;ROM&lt;/EM&gt; which &lt;EM&gt;flash.bin&lt;/EM&gt; partition he is supposed to verify and then to boot from (e.g. a bit in the OTP or something)?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aleksandar&lt;/P&gt;</description>
    <pubDate>Fri, 01 Oct 2021 10:57:52 GMT</pubDate>
    <dc:creator>aleksandar_niko</dc:creator>
    <dc:date>2021-10-01T10:57:52Z</dc:date>
    <item>
      <title>iMX 8M Nano - AB Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-Nano-AB-Boot/m-p/1349535#M180945</link>
      <description>&lt;P&gt;Hello support team,&lt;/P&gt;&lt;P&gt;we will work with a board based on the iMX 8M Nano processor and we are supposed to have a full AB Boot implemented. This would mean the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;two partitions which contain &lt;EM&gt;flash.bin&lt;/EM&gt; images&lt;/LI&gt;&lt;LI&gt;two &lt;EM&gt;boot&lt;/EM&gt; and &lt;EM&gt;root&lt;/EM&gt; partitions (though this isn't hard to do).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Question&lt;/STRONG&gt;: is there a way to tell the &lt;EM&gt;ROM&lt;/EM&gt; which &lt;EM&gt;flash.bin&lt;/EM&gt; partition he is supposed to verify and then to boot from (e.g. a bit in the OTP or something)?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aleksandar&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 10:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-Nano-AB-Boot/m-p/1349535#M180945</guid>
      <dc:creator>aleksandar_niko</dc:creator>
      <dc:date>2021-10-01T10:57:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 8M Nano - AB Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-Nano-AB-Boot/m-p/1349809#M180990</link>
      <description>&lt;P&gt;Hi Aleksandar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am afarid this is not feasible, there is no OTP bit to select partition to verify and then to boot from.&lt;/P&gt;
&lt;P&gt;There are primary and secondary images described in sect.6.1.6.1 Primary image offset and IVT offset,&lt;/P&gt;
&lt;P&gt;but secondary image is used only when primary boot image fails&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8MNRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Nano Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 03 Oct 2021 23:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8M-Nano-AB-Boot/m-p/1349809#M180990</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-10-03T23:37:00Z</dc:date>
    </item>
  </channel>
</rss>