<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 GPIO max read frequency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-max-read-frequency/m-p/1348482#M180832</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working with a 13 bit or 9 bit parallel camera interface with clocks at&amp;nbsp;48Mhz or&amp;nbsp;24Mhz. And I would like to know what is the GPIOs max reading frequency, or if there is another interface that the camera could be directly connected to, without the needs of extra hardware.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Platform:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;i.MX 8M Plus&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
    <pubDate>Wed, 29 Sep 2021 14:55:17 GMT</pubDate>
    <dc:creator>Eximius</dc:creator>
    <dc:date>2021-09-29T14:55:17Z</dc:date>
    <item>
      <title>GPIO max read frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-max-read-frequency/m-p/1348482#M180832</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working with a 13 bit or 9 bit parallel camera interface with clocks at&amp;nbsp;48Mhz or&amp;nbsp;24Mhz. And I would like to know what is the GPIOs max reading frequency, or if there is another interface that the camera could be directly connected to, without the needs of extra hardware.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Platform:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;i.MX 8M Plus&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 14:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-max-read-frequency/m-p/1348482#M180832</guid>
      <dc:creator>Eximius</dc:creator>
      <dc:date>2021-09-29T14:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO max read frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-max-read-frequency/m-p/1348612#M180839</link>
      <description>&lt;P&gt;Hi Eximius,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The max speed on GPIO can be found on the datasheet 3.5.1 General purpose I/O AC parameters:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxf63675_0-1632938019088.png" style="width: 591px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157920i93324E5B586279D7/image-dimensions/591x136?v=v2" width="591" height="136" role="button" title="nxf63675_0-1632938019088.png" alt="nxf63675_0-1632938019088.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nxf63675_0-1632938019088.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;And the processor has interfaces focus on a single Camera, MIPI CSI 1 can support up to 400/500 MHz pixel clock in the&lt;BR /&gt;Nominal/Overdrive mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 18:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-max-read-frequency/m-p/1348612#M180839</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-09-29T18:01:52Z</dc:date>
    </item>
  </channel>
</rss>