<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: gtest header files in SDK image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1347955#M180778</link>
    <description>&lt;P&gt;I think the package you need to install is "imx-gpu-sdk"&lt;/P&gt;</description>
    <pubDate>Wed, 29 Sep 2021 02:43:34 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2021-09-29T02:43:34Z</dc:date>
    <item>
      <title>gtest header files in SDK image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1344240#M180489</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've build imx8 SDK image for imx-image-full type and the gtest (googletest) header files are available in the SDK (usr/include/gtest/). However, when I try imx-image-core image type, the gtest header files are not present even I added googletest in&amp;nbsp; IMAGE_INSTALL. There is libgtest library, but no header files.&lt;/P&gt;&lt;P&gt;Any idea how to include gtest header files in the SDK image?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lijun&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 17:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1344240#M180489</guid>
      <dc:creator>lchen</dc:creator>
      <dc:date>2021-09-22T17:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: gtest header files in SDK image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1347955#M180778</link>
      <description>&lt;P&gt;I think the package you need to install is "imx-gpu-sdk"&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 02:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1347955#M180778</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-09-29T02:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: gtest header files in SDK image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1349622#M180955</link>
      <description>&lt;P&gt;Probably I was not clear in the original question. The issue is if I change googletest cmake to support shared library by:&lt;/P&gt;&lt;P&gt;EXTRA_OECMAKE = "-DBUILD_SHARED_LIBS=ON"&lt;/P&gt;&lt;P&gt;The header file is not included in the SDK image.&lt;/P&gt;&lt;P&gt;Turns out we have to change RDEPENDS_${PN}-dev += "${PN}-staticdev" to&lt;/P&gt;&lt;P&gt;RDEPENDS_${PN}-dev += "${PN}-dev"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lijun&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 15:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gtest-header-files-in-SDK-image/m-p/1349622#M180955</guid>
      <dc:creator>lchen</dc:creator>
      <dc:date>2021-10-01T15:00:08Z</dc:date>
    </item>
  </channel>
</rss>