<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1347655#M180753</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83098"&gt;@steffendoster&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The official kernel for iMX platforms can be found here : &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The latest release seems to be lf-5.10.52-2.1.0, and you can find the dts of 8MPLUS EVK here : &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.52-2.1.0&lt;/A&gt;. Possibly it is one of &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-ddr4-evk.dts?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;imx8mp-ddr4-evk.dts&lt;/A&gt; or &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.dts?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;imx8mp-evk.dts&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;BR /&gt;Khang&lt;/P&gt;</description>
    <pubDate>Tue, 28 Sep 2021 14:19:54 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2021-09-28T14:19:54Z</dc:date>
    <item>
      <title>Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1347574#M180744</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm stuck here with an 8MPLUS-BB Evalboard together with an 8MPLUS-LPD4-CPU-Module.&lt;/P&gt;&lt;P&gt;All I want is to compile a linux-kernel and devicetree which is able to display something on HDMI.&lt;/P&gt;&lt;P&gt;Sadly I had to realize that the board and the imx8mplus-evk.dts aren't fully compatible and that the board uses a LVDS-to-HDMI-Bridge which also isn't available in the kernel (&lt;A href="https://github.com/Freescale/linux-fslc)" target="_blank"&gt;https://github.com/Freescale/linux-fslc)&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Am I using the wrong Kernel? Which one is the correct kernel to properly bring up all the features of the board? Where can I get the sources for this board?&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 12:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1347574#M180744</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2021-09-28T12:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1347655#M180753</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83098"&gt;@steffendoster&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The official kernel for iMX platforms can be found here : &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The latest release seems to be lf-5.10.52-2.1.0, and you can find the dts of 8MPLUS EVK here : &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.52-2.1.0&lt;/A&gt;. Possibly it is one of &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-ddr4-evk.dts?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;imx8mp-ddr4-evk.dts&lt;/A&gt; or &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.dts?h=lf-5.10.52-2.1.0" target="_blank" rel="noopener"&gt;imx8mp-evk.dts&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;BR /&gt;Khang&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 14:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1347655#M180753</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2021-09-28T14:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1349159#M180895</link>
      <description>&lt;P&gt;Good!&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 13:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1349159#M180895</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-09-30T13:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1349874#M180997</link>
      <description>&lt;P&gt;Hi Khang,&lt;/P&gt;&lt;P&gt;yes, this was a great help. Thank you.&lt;/P&gt;&lt;P&gt;I downloaded and compiled the i.MX-Kernel and HDMI ran out of the box. Nice.&lt;BR /&gt;I hope the necessary drivers and devicetrees will find their way into mainline-kernel as well.&lt;/P&gt;&lt;P&gt;Greetings&lt;/P&gt;&lt;P&gt;Steffen&lt;/P&gt;</description>
      <pubDate>Mon, 04 Oct 2021 06:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-for-8MPLUS-BB-Evalboard-with-8MPLUS-LPD4-CPU-Module/m-p/1349874#M180997</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2021-10-04T06:01:19Z</dc:date>
    </item>
  </channel>
</rss>