<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to set up boot.scr?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347440#M180733</link>
    <description>&lt;P&gt;&lt;STRONG&gt;4.1.15-2.0.1&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;And here's other configs.&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Build Configuration:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;BB_VERSION = "1.30.0"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;BUILD_SYS = "x86_64-linux"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NATIVELSBSTRING = "Ubuntu-16.04"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MACHINE = "mys6ull14x14"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DISTRO = "myir-imx-fb"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DISTRO_VERSION = "4.1.15-2.0.1"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa7"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TARGET_FPU = "hard"&lt;/EM&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Sep 2021 09:02:41 GMT</pubDate>
    <dc:creator>totalit</dc:creator>
    <dc:date>2021-09-28T09:02:41Z</dc:date>
    <item>
      <title>How to set up boot.scr?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1346671#M180666</link>
      <description>&lt;P&gt;According the issue I described there&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344485/highlight/false" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344485/highlight/false&lt;/A&gt;&lt;BR /&gt;I built boot.scr with a startup sequence, so it's needed to be placed along with my image, despite NAND type. So how is it supposed to be done?&lt;/P&gt;&lt;P&gt;Usually I burn my .sdcard image via "sudo dd if=core-image-base-mys6ull14x14.rootfs.sdcard of=/dev/sdb1 bs=4M". Any way to include boot.scr into .sdcard?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Sep 2021 09:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1346671#M180666</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-27T09:13:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up boot.scr?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347107#M180695</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what bsp used in the case.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 00:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347107#M180695</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-28T00:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up boot.scr?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347440#M180733</link>
      <description>&lt;P&gt;&lt;STRONG&gt;4.1.15-2.0.1&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;And here's other configs.&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Build Configuration:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;BB_VERSION = "1.30.0"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;BUILD_SYS = "x86_64-linux"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NATIVELSBSTRING = "Ubuntu-16.04"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MACHINE = "mys6ull14x14"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DISTRO = "myir-imx-fb"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DISTRO_VERSION = "4.1.15-2.0.1"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa7"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TARGET_FPU = "hard"&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 09:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347440#M180733</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-28T09:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up boot.scr?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347494#M180737</link>
      <description>&lt;P&gt;one can look at&lt;/P&gt;
&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/29342821/creating-boot-scr-for-u-boot" target="_blank"&gt;https://stackoverflow.com/questions/29342821/creating-boot-scr-for-u-boot&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 10:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347494#M180737</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-28T10:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up boot.scr?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347508#M180738</link>
      <description>&lt;P&gt;I've already compile a boot.scr file, now I need to put it on boot SD card. What's the proper way to perform it?&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 10:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-boot-scr/m-p/1347508#M180738</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-28T10:30:11Z</dc:date>
    </item>
  </channel>
</rss>