<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx RT1160 increase NCACHE memory region in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-RT1160-increase-NCACHE-memory-region/m-p/1347081#M180690</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have an 1160 evk, with what I assume has two 256Mb Ram chips.&amp;nbsp; I am running the camera yuv sdk demo, and I wanted to increase the NCACHE region to get a larger image buffer (8 3Mb frames).&amp;nbsp; I tried increasing the size from 0x10000000 to 0x20000000 (16Mb to 32), but the program crashes.&amp;nbsp; Is there anything else I need to do to increase the memory availability?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Ed&lt;/P&gt;</description>
    <pubDate>Mon, 27 Sep 2021 21:57:18 GMT</pubDate>
    <dc:creator>Cococarbine</dc:creator>
    <dc:date>2021-09-27T21:57:18Z</dc:date>
    <item>
      <title>i.mx RT1160 increase NCACHE memory region</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-RT1160-increase-NCACHE-memory-region/m-p/1347081#M180690</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have an 1160 evk, with what I assume has two 256Mb Ram chips.&amp;nbsp; I am running the camera yuv sdk demo, and I wanted to increase the NCACHE region to get a larger image buffer (8 3Mb frames).&amp;nbsp; I tried increasing the size from 0x10000000 to 0x20000000 (16Mb to 32), but the program crashes.&amp;nbsp; Is there anything else I need to do to increase the memory availability?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Ed&lt;/P&gt;</description>
      <pubDate>Mon, 27 Sep 2021 21:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx-RT1160-increase-NCACHE-memory-region/m-p/1347081#M180690</guid>
      <dc:creator>Cococarbine</dc:creator>
      <dc:date>2021-09-27T21:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx RT1160 increase NCACHE memory region</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-RT1160-increase-NCACHE-memory-region/m-p/1347359#M180725</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1）Is there anything else I need to do to increase the memory availability?&lt;BR /&gt;-- As we know, the the MIMXRT1160-EVK board has two W9825G6KH, it means that the total size of the on-board SDRAM is 64 MB.&lt;BR /&gt;In the below figure, it consist of two parts: BOARD_SDRAM and NCACHE_REGION, when you increase the size of NCACHE_REGION to 32 MB from 16 MB, BOARD_SDRAM needs to decrease the same size.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeremyzhou_0-1632814883006.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157657iDE1C82BB0FEFCC18/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jeremyzhou_0-1632814883006.png" alt="jeremyzhou_0-1632814883006.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 07:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx-RT1160-increase-NCACHE-memory-region/m-p/1347359#M180725</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-09-28T07:41:41Z</dc:date>
    </item>
  </channel>
</rss>